<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MX7 USB - initialize but do not use USB Port</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX7-USB-initialize-but-do-not-use-USB-Port/m-p/829699#M127477</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you are correct, additionally capacitor at VDD_USB_OTGx_1P0_CAP&lt;/P&gt;&lt;P&gt;is needed for normal usb operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Aug 2018 23:17:53 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-08-07T23:17:53Z</dc:date>
    <item>
      <title>MX7 USB - initialize but do not use USB Port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7-USB-initialize-but-do-not-use-USB-Port/m-p/829698#M127476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for a customer I have developed two different hardware versions of bascially the same product.&lt;/P&gt;&lt;P&gt;One difference between the two versions is the usage of the the USB OTG ports. One version uses both ports, the other uses just one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far, the USB OTG port that has not been used was not powered and had no external circuitry at all.&lt;/P&gt;&lt;P&gt;To allow my customer to use the same software on both versions (initializes borh ports) I would like to allow the unused USB port to be initialized in software. What is the minimal circuitry to allow this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess: Power USB_OTGx_VDDA_3P3_in, attach a capacitor to OSB_OTGx_VBUS and a resistor to USB_OTGx_REXT? or may i cut some of these even?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks and regards,&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 13:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7-USB-initialize-but-do-not-use-USB-Port/m-p/829698#M127476</guid>
      <dc:creator>demoniacmilk</dc:creator>
      <dc:date>2018-08-07T13:48:00Z</dc:date>
    </item>
    <item>
      <title>Re: MX7 USB - initialize but do not use USB Port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX7-USB-initialize-but-do-not-use-USB-Port/m-p/829699#M127477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you are correct, additionally capacitor at VDD_USB_OTGx_1P0_CAP&lt;/P&gt;&lt;P&gt;is needed for normal usb operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 23:17:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX7-USB-initialize-but-do-not-use-USB-Port/m-p/829699#M127477</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-07T23:17:53Z</dc:date>
    </item>
  </channel>
</rss>