<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Custom IMX7D Board Issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX7D-Board-Issues/m-p/829500#M127460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a custom SBC for my company using the reference of IMX7D. I am only designing the baseboard and will be using the SOM as it is. For that, here are some of my doubts on that,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Do i have to create a custom Android Things image to flash on my custom board ? Or the Android things image that i use on the IMX7D board will also work on my custom SBC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. How should i get a root acaess to the kernel of the IMX7D ? I am using a USB type Camera on the IMX7D, and for that i may have to install Linux Kernel drivers.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Dec 2018 03:52:55 GMT</pubDate>
    <dc:creator>yuganshbansal</dc:creator>
    <dc:date>2018-12-04T03:52:55Z</dc:date>
    <item>
      <title>Custom IMX7D Board Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX7D-Board-Issues/m-p/829500#M127460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a custom SBC for my company using the reference of IMX7D. I am only designing the baseboard and will be using the SOM as it is. For that, here are some of my doubts on that,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Do i have to create a custom Android Things image to flash on my custom board ? Or the Android things image that i use on the IMX7D board will also work on my custom SBC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. How should i get a root acaess to the kernel of the IMX7D ? I am using a USB type Camera on the IMX7D, and for that i may have to install Linux Kernel drivers.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 03:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-IMX7D-Board-Issues/m-p/829500#M127460</guid>
      <dc:creator>yuganshbansal</dc:creator>
      <dc:date>2018-12-04T03:52:55Z</dc:date>
    </item>
  </channel>
</rss>