<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6sll pm wakeup source ttymxc1</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6sll-pm-wakeup-source-ttymxc1/m-p/829431#M127435</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello to who it may concerned&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use my customized board, and configure the uart2&lt;/P&gt;&lt;P&gt;it can work normally&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and i hope it can be the wakeup source for the low power mode.&lt;/P&gt;&lt;P&gt;i set the echo enabled &amp;gt; wakeup for ttymxc1&lt;/P&gt;&lt;P&gt;but it does not work&lt;/P&gt;&lt;P&gt;(if i set the ttymxc0,it can wake up the system)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i check the&amp;nbsp;i.MX 6SLL Applications Processor&amp;nbsp;Reference Manual&lt;/P&gt;&lt;P&gt;it seemed it can only work in the debug uart(ttymxc0)&lt;/P&gt;&lt;P&gt;is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if i want use uart2(ttymxc1),is there a solution for it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;looking forward your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Dec 2018 05:48:55 GMT</pubDate>
    <dc:creator>ilyyxfe</dc:creator>
    <dc:date>2018-12-25T05:48:55Z</dc:date>
    <item>
      <title>imx6sll pm wakeup source ttymxc1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sll-pm-wakeup-source-ttymxc1/m-p/829431#M127435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello to who it may concerned&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use my customized board, and configure the uart2&lt;/P&gt;&lt;P&gt;it can work normally&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and i hope it can be the wakeup source for the low power mode.&lt;/P&gt;&lt;P&gt;i set the echo enabled &amp;gt; wakeup for ttymxc1&lt;/P&gt;&lt;P&gt;but it does not work&lt;/P&gt;&lt;P&gt;(if i set the ttymxc0,it can wake up the system)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i check the&amp;nbsp;i.MX 6SLL Applications Processor&amp;nbsp;Reference Manual&lt;/P&gt;&lt;P&gt;it seemed it can only work in the debug uart(ttymxc0)&lt;/P&gt;&lt;P&gt;is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if i want use uart2(ttymxc1),is there a solution for it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;looking forward your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Dec 2018 05:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sll-pm-wakeup-source-ttymxc1/m-p/829431#M127435</guid>
      <dc:creator>ilyyxfe</dc:creator>
      <dc:date>2018-12-25T05:48:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx6sll pm wakeup source ttymxc1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sll-pm-wakeup-source-ttymxc1/m-p/829432#M127436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i enabled the ttymxc0 and ttymxc1, both of them can wakeup the system.&lt;/P&gt;&lt;P&gt;if ttymxc0 disabled, ttymxc1 can not wake up the sys/&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2018 05:31:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sll-pm-wakeup-source-ttymxc1/m-p/829432#M127436</guid>
      <dc:creator>ilyyxfe</dc:creator>
      <dc:date>2018-12-28T05:31:44Z</dc:date>
    </item>
    <item>
      <title>Re: imx6sll pm wakeup source ttymxc1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sll-pm-wakeup-source-ttymxc1/m-p/829433#M127437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uart wake up procedure is described in sect.21.1.5 Unit Test&lt;/P&gt;&lt;P&gt;attached Linux Manual. Example of dts uart settings:&lt;/P&gt;&lt;P&gt;linux/arch/arm/boot/dts/imx6sll.dtsi&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sll.dtsi?h=imx_4.1.15_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sll.dtsi?h=imx_4.1.15_2.0.0_ga"&gt;imx6sll.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2018 11:25:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sll-pm-wakeup-source-ttymxc1/m-p/829433#M127437</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-29T11:25:00Z</dc:date>
    </item>
  </channel>
</rss>