<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RTC driver in imx6ull in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RTC-driver-in-imx6ull/m-p/829298#M127415</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no special driver for the PCF85263A timer. You can use the regular I2C driver to access the timer.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Aug 2018 10:12:18 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2018-08-28T10:12:18Z</dc:date>
    <item>
      <title>RTC driver in imx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-driver-in-imx6ull/m-p/829297#M127414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using imx6ull based board. In my design, I'm using an external RTC pcf85263a.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To integrate the device, I need a driver for pcf85263a. But it is not available in the 4.1.15 Linux version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you provide a Linux driver for the pcf85263a? Otherwise, suggest a suitable driver available in the above Linux version that can be used instead of pcf85263a driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 12:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-driver-in-imx6ull/m-p/829297#M127414</guid>
      <dc:creator>mathew_k_t</dc:creator>
      <dc:date>2018-08-27T12:46:47Z</dc:date>
    </item>
    <item>
      <title>Re: RTC driver in imx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-driver-in-imx6ull/m-p/829298#M127415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no special driver for the PCF85263A timer. You can use the regular I2C driver to access the timer.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 10:12:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-driver-in-imx6ull/m-p/829298#M127415</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-08-28T10:12:18Z</dc:date>
    </item>
  </channel>
</rss>