<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error while Bitbake in imx6ulevk in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-Bitbake-in-imx6ulevk/m-p/828847#M127371</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I have followed the steps mentioned in i.MX_Yocto_Project_User's_Guide.pdf ,After entering bitbake command i am getting an error as follows,&lt;/P&gt;&lt;P&gt;$ DISTRO=fsl-imx-x11 MACHINE=imx6ulevk source fsl-setup-release.sh -b build&lt;/P&gt;&lt;P&gt;$ bitbake fsl-image-validation-imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error as follows:&lt;/P&gt;&lt;P&gt;dd: failed to open '/home/linux/fsl-release-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/fsl-image-validation-imx/1.0-r0/deploy-fl-image-validation-imx-image-complete/fsl-image-validation-imx-imx6ulevk-20180628121043.rootfs.ext4': No such file or directory&lt;/P&gt;&lt;P&gt;ERROR: Task (/home/linux/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb:do_image_sdcard) failed with exit code '1'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can any one help me to solve this problem.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Prasad.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jun 2018 12:24:38 GMT</pubDate>
    <dc:creator>nagaprasadvasam</dc:creator>
    <dc:date>2018-06-28T12:24:38Z</dc:date>
    <item>
      <title>Error while Bitbake in imx6ulevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-Bitbake-in-imx6ulevk/m-p/828847#M127371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I have followed the steps mentioned in i.MX_Yocto_Project_User's_Guide.pdf ,After entering bitbake command i am getting an error as follows,&lt;/P&gt;&lt;P&gt;$ DISTRO=fsl-imx-x11 MACHINE=imx6ulevk source fsl-setup-release.sh -b build&lt;/P&gt;&lt;P&gt;$ bitbake fsl-image-validation-imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error as follows:&lt;/P&gt;&lt;P&gt;dd: failed to open '/home/linux/fsl-release-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/fsl-image-validation-imx/1.0-r0/deploy-fl-image-validation-imx-image-complete/fsl-image-validation-imx-imx6ulevk-20180628121043.rootfs.ext4': No such file or directory&lt;/P&gt;&lt;P&gt;ERROR: Task (/home/linux/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb:do_image_sdcard) failed with exit code '1'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can any one help me to solve this problem.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Prasad.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 12:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-Bitbake-in-imx6ulevk/m-p/828847#M127371</guid>
      <dc:creator>nagaprasadvasam</dc:creator>
      <dc:date>2018-06-28T12:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: Error while Bitbake in imx6ulevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-Bitbake-in-imx6ulevk/m-p/828848#M127372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Prasad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you still experiencing this issue? I would recommend doing a cleanall and then trying again, as it looks like some of the files that should have been generated cannot be found and making a clean would force bitbake to generate it again: bitbake -c cleanall &amp;lt;image&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 19:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-Bitbake-in-imx6ulevk/m-p/828848#M127372</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-07-24T19:18:16Z</dc:date>
    </item>
  </channel>
</rss>