<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue on Camera: Multiple Frames on single screen in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-Camera-Multiple-Frames-on-single-screen/m-p/828510#M127337</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, the camera OV5467 is not supported by our BSP. However, you can try to use the OV5460 model.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the inconveniences.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jul 2018 15:03:18 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-07-23T15:03:18Z</dc:date>
    <item>
      <title>Issue on Camera: Multiple Frames on single screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-Camera-Multiple-Frames-on-single-screen/m-p/828509#M127336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;We are using OV5647 MIPI camera on imx6 platform with Android 7.1.2 BSP. We have bring-up the camera on linux level and it's working perfectly on sample linux test application (mxc_v4l2_capture). Then I integrated this camera support on Android HAL. Now I'm able to view the camera data on default android application. But we are getting same camera data in 20 frames in a single screen, I have attached screenshot of captured image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please support on this.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aravinth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 11:49:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-on-Camera-Multiple-Frames-on-single-screen/m-p/828509#M127336</guid>
      <dc:creator>aravinthkumarja</dc:creator>
      <dc:date>2018-06-28T11:49:53Z</dc:date>
    </item>
    <item>
      <title>Re: Issue on Camera: Multiple Frames on single screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-Camera-Multiple-Frames-on-single-screen/m-p/828510#M127337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, the camera OV5467 is not supported by our BSP. However, you can try to use the OV5460 model.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the inconveniences.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 15:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-on-Camera-Multiple-Frames-on-single-screen/m-p/828510#M127337</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-07-23T15:03:18Z</dc:date>
    </item>
  </channel>
</rss>