<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLVDS display problem with kernel 3.14.28</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-display-problem-with-kernel-3-14-28/m-p/827812#M127246</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to add support for LVDS display to i.MX6DL board running 3.14.28 kernel, but the picture is distorted. See attached photos for details (in boot screen photo dark areas are supposed to be solid black).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same display works fine with kernel imx_4.1.15_2.0.0_ga, but unfortunately there's a requirement to make it work with 3.14.28 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've used exactly the same relevant DT nodes from 4.1.15 kernel (attached in a fido_display.dts file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is strange: setting resolution to 1920x1080 (proper/desired resolution is 800x480) and enabling split mode fixes the picture (see fbtest_ok.JPG), but it doesn't fit the display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions as to where to look: missing commit(s) to one of IPU drivers, DT properties, etc?&lt;/P&gt;&lt;P&gt;Also what kind of setting mismatch could produce picture distortion we are observing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2018 12:56:11 GMT</pubDate>
    <dc:creator>ivandrobyshevsk</dc:creator>
    <dc:date>2018-07-18T12:56:11Z</dc:date>
    <item>
      <title>LVDS display problem with kernel 3.14.28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-display-problem-with-kernel-3-14-28/m-p/827812#M127246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to add support for LVDS display to i.MX6DL board running 3.14.28 kernel, but the picture is distorted. See attached photos for details (in boot screen photo dark areas are supposed to be solid black).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same display works fine with kernel imx_4.1.15_2.0.0_ga, but unfortunately there's a requirement to make it work with 3.14.28 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've used exactly the same relevant DT nodes from 4.1.15 kernel (attached in a fido_display.dts file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is strange: setting resolution to 1920x1080 (proper/desired resolution is 800x480) and enabling split mode fixes the picture (see fbtest_ok.JPG), but it doesn't fit the display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions as to where to look: missing commit(s) to one of IPU drivers, DT properties, etc?&lt;/P&gt;&lt;P&gt;Also what kind of setting mismatch could produce picture distortion we are observing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 12:56:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-display-problem-with-kernel-3-14-28/m-p/827812#M127246</guid>
      <dc:creator>ivandrobyshevsk</dc:creator>
      <dc:date>2018-07-18T12:56:11Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS display problem with kernel 3.14.28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-display-problem-with-kernel-3-14-28/m-p/827813#M127247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ivan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if recommended LDB Clock Switch Procedure was implemented as&lt;/P&gt;&lt;P&gt;recommended by EB821&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf" title="https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf"&gt;https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can try official nxp bsps described on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fsupport%2Fdeveloper-resources%2Frun-time-software%2Fi.mx-developer-resources%2Fi.mx-6series-i.mx-7series-software-and-development-tool-resources%3AIMX_SW" rel="nofollow" target="_blank"&gt;https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 01:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-display-problem-with-kernel-3-14-28/m-p/827813#M127247</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-19T01:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS display problem with kernel 3.14.28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-display-problem-with-kernel-3-14-28/m-p/827814#M127248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For whatever reason, clock speed had to be set two times faster compared to kernel 4.1.15. With higher speed picture looks good again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 10:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-display-problem-with-kernel-3-14-28/m-p/827814#M127248</guid>
      <dc:creator>ivandrobyshevsk</dc:creator>
      <dc:date>2018-07-26T10:40:15Z</dc:date>
    </item>
  </channel>
</rss>