<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX6 VPU (coder and decoder)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-VPU-coder-and-decoder/m-p/827754#M127230</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have replied to you in salesforce , any update, pls mail to me .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Jan 2019 09:21:38 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2019-01-03T09:21:38Z</dc:date>
    <item>
      <title>I.MX6 VPU (coder and decoder)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-VPU-coder-and-decoder/m-p/827753#M127229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Recently, we have a customer who always has problems when using vpu codec. Their requirements are generally as follows:&lt;/P&gt;&lt;P&gt;1) : JPG decoded into yuv422&lt;/P&gt;&lt;P&gt;2) : yuv422 is converted into yuv420,&lt;/P&gt;&lt;P&gt;3) : yuv420 is encoded as h264&lt;/P&gt;&lt;P&gt;The vpu library used by the client is libimxvpuapi-0.10.3 released on github&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/github.com/Freescale/libimxvpuapi" rel="nofollow" target="_blank"&gt;https://github.com/Freescale/libimxvpuapi&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The problems encountered are as follows:&lt;/P&gt;&lt;P&gt;1).JPEG decoding and releasing resources will cause a crash. The official website libimxvpuapi-0.10.3 version jpeg-dec-example is used&lt;/P&gt;&lt;P&gt;- &amp;gt; test&lt;/P&gt;&lt;P&gt;. / MXCCameraDemo - 1&lt;/P&gt;&lt;P&gt;2). Jpeg decoding and h264 encoding with libimxvpuapi-0.10.3 example from the official website will crash randomly if multiple threads are started and multiple instances are used at the same time&lt;/P&gt;&lt;P&gt;- &amp;gt; test&lt;/P&gt;&lt;P&gt;. / MXCCameraDemo - 2&lt;/P&gt;&lt;P&gt;3) IPU transcoding 1280*720P from YUV422 to YUV420 will cause the display module to hang and the screen to be white (it needs to run for a period of time, more than 5 minutes)&lt;/P&gt;&lt;P&gt;4). The CPU utilization rate is very high when decoding and encoding, so that inexplicable stuck and crashed when embedded into our main program&lt;/P&gt;&lt;P&gt;5). Sometimes there will be lag in codec, and the same data will be decoded and encoded in test&lt;/P&gt;&lt;P&gt;- &amp;gt; test&lt;/P&gt;&lt;P&gt;. / MXCCameraDemo - 3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Dec 2018 02:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-VPU-coder-and-decoder/m-p/827753#M127229</guid>
      <dc:creator>blackhuang</dc:creator>
      <dc:date>2018-12-24T02:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 VPU (coder and decoder)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-VPU-coder-and-decoder/m-p/827754#M127230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have replied to you in salesforce , any update, pls mail to me .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2019 09:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-VPU-coder-and-decoder/m-p/827754#M127230</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-01-03T09:21:38Z</dc:date>
    </item>
  </channel>
</rss>