<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDo we need to control impedance of CAN BUS ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Do-we-need-to-control-impedance-of-CAN-BUS/m-p/826987#M127154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gary_bisson"&gt;gary_bisson&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My hardware design is most similar to nitrogen6_max development board and I have included CAN BUS port to my custom design which is similar to Sabre Lite board (CAN BUS).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my memory layout I controlled impedance as 100 Ohms for differential pair and 50 Ohms for single ended signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in Sabre lite schematic design CAN BUS is not differential pair. Is that correct ? Don't we need to control impedance of the CAN BUS traces ? If yes what is the impedance value ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kulunu.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Aug 2018 06:27:07 GMT</pubDate>
    <dc:creator>peteramond</dc:creator>
    <dc:date>2018-08-07T06:27:07Z</dc:date>
    <item>
      <title>Do we need to control impedance of CAN BUS ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-we-need-to-control-impedance-of-CAN-BUS/m-p/826987#M127154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gary_bisson"&gt;gary_bisson&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My hardware design is most similar to nitrogen6_max development board and I have included CAN BUS port to my custom design which is similar to Sabre Lite board (CAN BUS).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my memory layout I controlled impedance as 100 Ohms for differential pair and 50 Ohms for single ended signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in Sabre lite schematic design CAN BUS is not differential pair. Is that correct ? Don't we need to control impedance of the CAN BUS traces ? If yes what is the impedance value ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kulunu.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 06:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-we-need-to-control-impedance-of-CAN-BUS/m-p/826987#M127154</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2018-08-07T06:27:07Z</dc:date>
    </item>
    <item>
      <title>Re: Do we need to control impedance of CAN BUS ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-we-need-to-control-impedance-of-CAN-BUS/m-p/826988#M127155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The standard specifies a two-wire differential bus;&amp;nbsp; the characteristic line impedance is 120 Ohm. &lt;/P&gt;&lt;P&gt;The i.MX6 Design recommendations about 100 Ohms for differential pair is quite reasonable for FlexCAN&lt;/P&gt;&lt;P&gt;too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 09:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-we-need-to-control-impedance-of-CAN-BUS/m-p/826988#M127155</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-08-07T09:42:20Z</dc:date>
    </item>
  </channel>
</rss>