<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Inflexion demo hangs at IFXF_Initialize function. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-demo-hangs-at-IFXF-Initialize-function/m-p/211100#M12715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have built the inflexion demo in the Linux environment.&lt;/P&gt;&lt;P&gt;After the successful build,&amp;nbsp; I run the exe on a target, but the problem is the exe runs till I get a print&lt;/P&gt;&lt;P&gt;"Running on IMX 53" and then it hangs.&lt;/P&gt;&lt;P&gt;The problem is most probably is happening in engine config part of IFXF_Initialize function in framework_linux_generic.c. But i am unable proceed further.&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Sharan K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Feb 2012 03:53:48 GMT</pubDate>
    <dc:creator>SharanK</dc:creator>
    <dc:date>2012-02-15T03:53:48Z</dc:date>
    <item>
      <title>Inflexion demo hangs at IFXF_Initialize function.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-demo-hangs-at-IFXF-Initialize-function/m-p/211100#M12715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have built the inflexion demo in the Linux environment.&lt;/P&gt;&lt;P&gt;After the successful build,&amp;nbsp; I run the exe on a target, but the problem is the exe runs till I get a print&lt;/P&gt;&lt;P&gt;"Running on IMX 53" and then it hangs.&lt;/P&gt;&lt;P&gt;The problem is most probably is happening in engine config part of IFXF_Initialize function in framework_linux_generic.c. But i am unable proceed further.&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Sharan K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2012 03:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-demo-hangs-at-IFXF-Initialize-function/m-p/211100#M12715</guid>
      <dc:creator>SharanK</dc:creator>
      <dc:date>2012-02-15T03:53:48Z</dc:date>
    </item>
  </channel>
</rss>