<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Boot without external RTC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-without-external-RTC/m-p/826799#M127125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we designed our own i.MX 8M Hardware and it is not possible to boot without an external 32kHz clock. When we connect a external 32kHz clock there are no Bootproblems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Datasheet says: "When an external RTC clock input is not present, the 32 kHz clock for internal logic is generated by the 25 MHz oscillator".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a known issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jun 2018 14:19:40 GMT</pubDate>
    <dc:creator>AdrianMerrath</dc:creator>
    <dc:date>2018-06-28T14:19:40Z</dc:date>
    <item>
      <title>Boot without external RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-without-external-RTC/m-p/826799#M127125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we designed our own i.MX 8M Hardware and it is not possible to boot without an external 32kHz clock. When we connect a external 32kHz clock there are no Bootproblems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Datasheet says: "When an external RTC clock input is not present, the 32 kHz clock for internal logic is generated by the 25 MHz oscillator".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a known issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 14:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-without-external-RTC/m-p/826799#M127125</guid>
      <dc:creator>AdrianMerrath</dc:creator>
      <dc:date>2018-06-28T14:19:40Z</dc:date>
    </item>
    <item>
      <title>Re: Boot without external RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-without-external-RTC/m-p/826800#M127126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; External RTC clock is mandatory.&lt;/P&gt;&lt;P&gt;All three clock sources (RTC clock,&amp;nbsp;&amp;nbsp;XTAL 25M,&amp;nbsp;XTAL 27M) are mentioned explicitly&lt;/P&gt;&lt;P&gt;as must be running in the i.MX8M Hardware Developer’s Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="line-height: 15.0pt;"&gt;&amp;nbsp; The Datasheet(s) should be&lt;SPAN style="font-size: 10.5pt; font-family: 'Helvetica',sans-serif; color: #666666;"&gt; updated in order to remove the following statement:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="line-height: 15.0pt;"&gt;&lt;SPAN style="font-size: 10.5pt; font-family: 'Helvetica',sans-serif; color: #666666;"&gt;"When an external RTC clock input is not present, the 32 kHz clock for internal logic &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="line-height: 15.0pt;"&gt;&lt;SPAN style="font-size: 10.5pt; font-family: 'Helvetica',sans-serif; color: #666666;"&gt;is generated by the 25 MHz oscillator".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 06:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-without-external-RTC/m-p/826800#M127126</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-06-29T06:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: Boot without external RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-without-external-RTC/m-p/826801#M127127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you very much for your help. This is an important information for our redesign.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 07:24:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-without-external-RTC/m-p/826801#M127127</guid>
      <dc:creator>AdrianMerrath</dc:creator>
      <dc:date>2018-06-29T07:24:40Z</dc:date>
    </item>
  </channel>
</rss>