<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SSD boot on iMX8 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SSD-boot-on-iMX8/m-p/826616#M127093</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Motti&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from other unsupported devices one can use plugin method (first boot from supported&lt;/P&gt;&lt;P&gt;device) described in sect.6.1.7 Plugin image i.MX8M Reference Manual.&lt;/P&gt;&lt;P&gt;Unfortunately there is no way to add boot option from SSD directly, as boot&lt;/P&gt;&lt;P&gt;sequence is hardcoded in ROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Dec 2018 07:31:09 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-12-03T07:31:09Z</dc:date>
    <item>
      <title>SSD boot on iMX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SSD-boot-on-iMX8/m-p/826615#M127092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the Reference Manual, it supports below boot devices:&lt;/P&gt;&lt;P&gt;• SD/MMC&lt;BR /&gt;• NAND flash&lt;BR /&gt;• FlexSPI NOR flash (on FlexSPI0)&lt;BR /&gt;• Serial downloader support on USB 2.0 OTG and USB 3.0 (as 2.0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that there is no boot for SSD (SATA or PCIe).&lt;/P&gt;&lt;P&gt;On the contrary, iMX6 Sabre AI seems to support booting on SATA hard drive per mentioned in &lt;A href="https://community.nxp.com/docs/DOC-328196"&gt;https://community.nxp.com/docs/DOC-328196&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Due to cost issue, we really want to remove the eMMC and boot from SSD directly.&lt;/P&gt;&lt;P&gt;Is there any way we can do that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Dec 2018 03:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SSD-boot-on-iMX8/m-p/826615#M127092</guid>
      <dc:creator>motting</dc:creator>
      <dc:date>2018-12-03T03:16:54Z</dc:date>
    </item>
    <item>
      <title>Re: SSD boot on iMX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SSD-boot-on-iMX8/m-p/826616#M127093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Motti&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from other unsupported devices one can use plugin method (first boot from supported&lt;/P&gt;&lt;P&gt;device) described in sect.6.1.7 Plugin image i.MX8M Reference Manual.&lt;/P&gt;&lt;P&gt;Unfortunately there is no way to add boot option from SSD directly, as boot&lt;/P&gt;&lt;P&gt;sequence is hardcoded in ROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Dec 2018 07:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SSD-boot-on-iMX8/m-p/826616#M127093</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-03T07:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: SSD boot on iMX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SSD-boot-on-iMX8/m-p/1492606#M192779</link>
      <description>&lt;P&gt;Did you ever find a solution to this? I am running into the same problem.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 16:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SSD-boot-on-iMX8/m-p/1492606#M192779</guid>
      <dc:creator>jonk4m</dc:creator>
      <dc:date>2022-07-20T16:54:12Z</dc:date>
    </item>
  </channel>
</rss>