<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can I use eMMC chip From ISS instead of SDIN5C2-8G which is obsolete in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-eMMC-chip-From-ISS-instead-of-SDIN5C2-8G-which-is/m-p/826136#M127035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&amp;nbsp; i am designing new board based on I.MX6 Dual Lite SoC, i want to use 1mm pitch package which is available from &lt;STRONG&gt;INTEGRATED SILICON SOLUTIONS&lt;/STRONG&gt; and part no is&amp;nbsp;&lt;STRONG&gt;IS21ES016G&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;please suggest me can i use this or not other wise tell me is there any eMMC flash with 1MM pitch&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards and Thanks&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Aug 2018 10:29:37 GMT</pubDate>
    <dc:creator>saida</dc:creator>
    <dc:date>2018-08-07T10:29:37Z</dc:date>
    <item>
      <title>Can I use eMMC chip From ISS instead of SDIN5C2-8G which is obsolete</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-eMMC-chip-From-ISS-instead-of-SDIN5C2-8G-which-is/m-p/826136#M127035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&amp;nbsp; i am designing new board based on I.MX6 Dual Lite SoC, i want to use 1mm pitch package which is available from &lt;STRONG&gt;INTEGRATED SILICON SOLUTIONS&lt;/STRONG&gt; and part no is&amp;nbsp;&lt;STRONG&gt;IS21ES016G&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;please suggest me can i use this or not other wise tell me is there any eMMC flash with 1MM pitch&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards and Thanks&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 10:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-eMMC-chip-From-ISS-instead-of-SDIN5C2-8G-which-is/m-p/826136#M127035</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2018-08-07T10:29:37Z</dc:date>
    </item>
  </channel>
</rss>