<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Error build image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-build-image/m-p/825871#M127001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ruslan Bichihin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that you are using a CL-SOM-iMX8 - NXP i.MX8 System-on-Module from Compulab. I would recommend looking if there is a more stable release as it looks like you are using a beta BSP. I would also refer to documentation and support from Compulab, as they are the owners of this BSP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jul 2018 17:06:14 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-07-20T17:06:14Z</dc:date>
    <item>
      <title>Error build image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-build-image/m-p/825870#M127000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello every one&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try build image by Yocto, this my logs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.36.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "debian-8"&lt;BR /&gt;TARGET_SYS = "aarch64-poky-linux"&lt;BR /&gt;MACHINE = "cl-som-imx8"&lt;BR /&gt;DISTRO = "fsl-imx-xwayland"&lt;BR /&gt;DISTRO_VERSION = "4.9.88-2.2.0_8qxp_beta2"&lt;BR /&gt;TUNE_FEATURES = "aarch64"&lt;BR /&gt;TARGET_FPU = ""&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:fdeecc901196bbccd7c5b1ea4268a2cf56764a62"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-freescale = "HEAD:d6141ea291a1ac9ab8fb1dd1110d408f840fda57"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:62de01743c9233ea718de22991c47b73a78b4857"&lt;BR /&gt;meta-freescale-distro = "HEAD:0ec6d7e206705702b5b534611754de0787f92b72"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk = "HEAD:3d345c4dfc748e44efd30e6310c314b2498ea6f4"&lt;BR /&gt;meta-browser = "HEAD:d6f9aed41c73b75a97d71bff060b03a66ee087b1"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-python &lt;BR /&gt;meta-filesystems = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-qt5 = "HEAD:cfe02f26de53e5c20e6f9555059cbaaf5ab9b22f"&lt;BR /&gt;meta-compulab = "devel:d226d9c232eac7153267d54a00b90f6bb828b4fe"&lt;BR /&gt;meta-xfce = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-compulab-imx8 = "devel_ga:9c702be423ae39aea8f29208cbd838528d4ce1e9"&lt;/P&gt;&lt;P&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;NOTE: Running task 1 of 10149 (/usr/imx8/fsl-release-bsp/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.65.bb:do_fetch)&lt;BR /&gt;NOTE: Running task 2 of 10149 (/usr/imx8/fsl-release-bsp/sources/poky/meta/recipes-extended/texinfo-dummy-native/texinfo-dummy-native.bb:do_fetch)&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;NOTE: Running task 676 of 10149 (/usr/imx8/fsl-release-bsp/sources/poky/meta/recipes-core/kbd/kbd_2.0.4.bb:do_fetch)&lt;BR /&gt;NOTE: recipe gawk-4.1.4-r0: task do_patch: Started&lt;BR /&gt;&lt;STRONG&gt;ERROR: linux-imx-4.9.88-r0 do_patch: Command Error: 'quilt --quiltrc /usr/imx8/fsl-release-bsp/build-cl-som-imx8-fsl-imx-xwayland/tmp/work/cl_som_imx8-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/etc/quiltrc push' exited with 0 Output:&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Applying patch 0030-nxp-pcie-External-OSC-handling.patch&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;patching file drivers/pci/host/pci-imx6.c&lt;/STRONG&gt;&lt;BR /&gt;Hunk #1 FAILED at 79.&lt;BR /&gt;Hunk #2 FAILED at 1064.&lt;BR /&gt;Hunk #3 FAILED at 2219.&lt;BR /&gt;3 out of 3 hunks FAILED -- rejects in file drivers/pci/host/pci-imx6.c&lt;BR /&gt;&lt;STRONG&gt;Patch 0030-nxp-pcie-External-OSC-handling.patch does not apply&lt;/STRONG&gt; (enforce with -f)&lt;BR /&gt;ERROR: linux-imx-4.9.88-r0 do_patch: Function failed: patch_do_patch&lt;BR /&gt;ERROR: Logfile of failure stored in: /usr/imx8/fsl-release-bsp/build-cl-som-imx8-fsl-imx-xwayland/tmp/work/cl_som_imx8-poky-linux/linux-imx/4.9.88-r0/temp/log.do_patch.15387&lt;BR /&gt;NOTE: recipe linux-imx-4.9.88-r0: task do_patch: Failed&lt;BR /&gt;ERROR: Task (/usr/imx8/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.9.88.bb:do_patch) failed with exit code '1'&lt;BR /&gt;NOTE: Running task 677 of 10149 (/usr/imx8/fsl-release-bsp/sources/poky/meta/recipes-graphics/xorg-lib/libxv_1.0.11.bb:do_fetch)&lt;BR /&gt;NOTE: recipe kbd-2.0.4-r0: task do_fetch: Started&lt;BR /&gt;NOTE: recipe gconf-3.2.6-r0: task do_fetch: Succeeded&lt;BR /&gt;NOTE: recipe gawk-4.1.4-r0: task do_patch: Succeeded&lt;BR /&gt;NOTE: recipe libxv-1.0.11-r0: task do_fetch: Started&lt;BR /&gt;NOTE: recipe kbd-2.0.4-r0: task do_fetch: Succeeded&lt;BR /&gt;NOTE: recipe e2fsprogs-1.43.5-r0: task do_patch: Succeeded&lt;BR /&gt;NOTE: recipe automake-native-1.15.1-r0: task do_configure: Succeeded&lt;BR /&gt;NOTE: recipe libxv-1.0.11-r0: task do_fetch: Succeeded&lt;BR /&gt;NOTE: recipe protobuf-native-3.5.1+gitAUTOINC+106ffc04be-r0: task do_fetch: Succeeded&lt;BR /&gt;NOTE: recipe protobuf-3.5.1+gitAUTOINC+106ffc04be-r0: task do_fetch: Succeeded&lt;BR /&gt;NOTE: Tasks Summary: Attempted 677 tasks of which 0 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;===================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe enybody know, why path&amp;nbsp;&lt;STRONG&gt;0030-nxp-pcie-External-OSC-handling.patch does not apply ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;How i can reslove this problem?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Tkanks!&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 10:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-build-image/m-p/825870#M127000</guid>
      <dc:creator>ruslan_g</dc:creator>
      <dc:date>2018-07-18T10:30:33Z</dc:date>
    </item>
    <item>
      <title>Re: Error build image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-build-image/m-p/825871#M127001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ruslan Bichihin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that you are using a CL-SOM-iMX8 - NXP i.MX8 System-on-Module from Compulab. I would recommend looking if there is a more stable release as it looks like you are using a beta BSP. I would also refer to documentation and support from Compulab, as they are the owners of this BSP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 17:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-build-image/m-p/825871#M127001</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-07-20T17:06:14Z</dc:date>
    </item>
  </channel>
</rss>