<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックuboot plugin mode used in HAB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uboot-plugin-mode-used-in-HAB/m-p/825803#M126987</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My project want to use seucre boot at imx6d&lt;/P&gt;&lt;P&gt;Current project use mx6q_4x_mt41j128.cfg with CONFIG_USE_PLUGIN&lt;/P&gt;&lt;P&gt;But It seem if I want to use thesecureboot&amp;nbsp; fuction.I need undef CONFIG_USE_PLUGIN&lt;/P&gt;&lt;P&gt;1.Could it have some introduce about the uboot plugin mode ?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" style="box-sizing: border-box;"&gt;2.&lt;/SPAN&gt;If I want to add the secure boot fuse with uboot plugin mode.what could I do ?&lt;BR /&gt;3.if I use the DCDmode.How can I trans the plugin config to cfg file&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2018 10:02:14 GMT</pubDate>
    <dc:creator>liuhao1</dc:creator>
    <dc:date>2018-07-18T10:02:14Z</dc:date>
    <item>
      <title>uboot plugin mode used in HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-plugin-mode-used-in-HAB/m-p/825803#M126987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My project want to use seucre boot at imx6d&lt;/P&gt;&lt;P&gt;Current project use mx6q_4x_mt41j128.cfg with CONFIG_USE_PLUGIN&lt;/P&gt;&lt;P&gt;But It seem if I want to use thesecureboot&amp;nbsp; fuction.I need undef CONFIG_USE_PLUGIN&lt;/P&gt;&lt;P&gt;1.Could it have some introduce about the uboot plugin mode ?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" style="box-sizing: border-box;"&gt;2.&lt;/SPAN&gt;If I want to add the secure boot fuse with uboot plugin mode.what could I do ?&lt;BR /&gt;3.if I use the DCDmode.How can I trans the plugin config to cfg file&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 10:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-plugin-mode-used-in-HAB/m-p/825803#M126987</guid>
      <dc:creator>liuhao1</dc:creator>
      <dc:date>2018-07-18T10:02:14Z</dc:date>
    </item>
    <item>
      <title>Re: uboot plugin mode used in HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-plugin-mode-used-in-HAB/m-p/825804#M126988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi liuhao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please create service request for obtaining additional information&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 23:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-plugin-mode-used-in-HAB/m-p/825804#M126988</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-18T23:09:54Z</dc:date>
    </item>
  </channel>
</rss>