<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックNAND Flash and GPIO Boot Overides</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-and-GPIO-Boot-Overides/m-p/210950#M12669</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Folks,&lt;/P&gt;&lt;P&gt;I'm designing a new board based off the QSB. &amp;nbsp;I am adding two NAND flash chips and connecting them to the EIM_DA[7..0] pins. &amp;nbsp; &amp;nbsp;These are the same pins used for some of the GPIO boot overides which are sampled at boot when using boot mode 0x00. &amp;nbsp; If I use 10k pull-ups/downs on these pins to select my desired boot config, will it interfere with normal NAND operation? &amp;nbsp; Should I instead configure my NAND to use the PATA lines? &amp;nbsp;Or should I just not use internal boot and boot from fuses instead?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Suggestions appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Mark Roy&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Feb 2012 18:36:50 GMT</pubDate>
    <dc:creator>MarkRoy</dc:creator>
    <dc:date>2012-02-14T18:36:50Z</dc:date>
    <item>
      <title>NAND Flash and GPIO Boot Overides</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-and-GPIO-Boot-Overides/m-p/210950#M12669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Folks,&lt;/P&gt;&lt;P&gt;I'm designing a new board based off the QSB. &amp;nbsp;I am adding two NAND flash chips and connecting them to the EIM_DA[7..0] pins. &amp;nbsp; &amp;nbsp;These are the same pins used for some of the GPIO boot overides which are sampled at boot when using boot mode 0x00. &amp;nbsp; If I use 10k pull-ups/downs on these pins to select my desired boot config, will it interfere with normal NAND operation? &amp;nbsp; Should I instead configure my NAND to use the PATA lines? &amp;nbsp;Or should I just not use internal boot and boot from fuses instead?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Suggestions appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Mark Roy&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2012 18:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-and-GPIO-Boot-Overides/m-p/210950#M12669</guid>
      <dc:creator>MarkRoy</dc:creator>
      <dc:date>2012-02-14T18:36:50Z</dc:date>
    </item>
  </channel>
</rss>