<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CSF description language input parameter capability? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CSF-description-language-input-parameter-capability/m-p/823670#M126689</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In order to fully automate the code signing process,&amp;nbsp;we would like to pass in the byte count to sign, as a parameter to the code signing tool binary, for the CSF command [Authenticate Data] like so:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Authenticate Data]&lt;/P&gt;&lt;P&gt;Verification index = 2&lt;BR /&gt;Blocks = 0x80000400 0x400&amp;nbsp;$(SignatureSize) "./image.bin"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code signing tool user's guide does not advertise any such capability.&amp;nbsp; Still, I wonder if (for example) an environment variable can be interpreted by the CSF script parser.&amp;nbsp;&amp;nbsp;Does the CSF interpreter&amp;nbsp;facilitate input parameters by any means?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Stephen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Nov 2018 17:57:11 GMT</pubDate>
    <dc:creator>stephenbialkows</dc:creator>
    <dc:date>2018-11-30T17:57:11Z</dc:date>
    <item>
      <title>CSF description language input parameter capability?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSF-description-language-input-parameter-capability/m-p/823670#M126689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In order to fully automate the code signing process,&amp;nbsp;we would like to pass in the byte count to sign, as a parameter to the code signing tool binary, for the CSF command [Authenticate Data] like so:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Authenticate Data]&lt;/P&gt;&lt;P&gt;Verification index = 2&lt;BR /&gt;Blocks = 0x80000400 0x400&amp;nbsp;$(SignatureSize) "./image.bin"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code signing tool user's guide does not advertise any such capability.&amp;nbsp; Still, I wonder if (for example) an environment variable can be interpreted by the CSF script parser.&amp;nbsp;&amp;nbsp;Does the CSF interpreter&amp;nbsp;facilitate input parameters by any means?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Stephen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2018 17:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSF-description-language-input-parameter-capability/m-p/823670#M126689</guid>
      <dc:creator>stephenbialkows</dc:creator>
      <dc:date>2018-11-30T17:57:11Z</dc:date>
    </item>
  </channel>
</rss>