<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: gst-fsl-plugin build failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/gst-fsl-plugin-build-failed/m-p/210944#M12668</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The &lt;STRONG&gt;peq_ppp_interface.h &lt;/STRONG&gt;is not in the same directory as the plugins, but is located in codec package fsl-mm-codeclib-2.0.3-2.tar.gz (fsl-mm-codeclib-2.0.3\ghdr\). you can check if it is existent in the codec package.&lt;/P&gt;&lt;P&gt;Please start with a clean build.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Oct 2012 06:53:57 GMT</pubDate>
    <dc:creator>PhilChen</dc:creator>
    <dc:date>2012-10-09T06:53:57Z</dc:date>
    <item>
      <title>gst-fsl-plugin build failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gst-fsl-plugin-build-failed/m-p/210943#M12667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Ubuntu desktop 12.04 and LTIB to build the Gstreamer plugin for i.mx 53 qsb.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am getting the following error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mfw_gst_audio_pp.c:47:31: error: peq_ppp_interface.h: No such file or directory&lt;/STRONG&gt;&lt;BR /&gt;In file included from mfw_gst_audio_pp.c:54:&lt;BR /&gt;mfw_gst_audio_pp.h:100: error: expected specifier-qualifier-list before 'PEQ_PPP_Config'&lt;BR /&gt;mfw_gst_audio_pp.c:362: error: expected ')' before '*' token&lt;BR /&gt;mfw_gst_audio_pp.c: In function 'parametric_eq_set_parameter':&lt;BR /&gt;mfw_gst_audio_pp.c:408: error: 'PEQ_PL' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:408: error: (Each undeclared identifier is reported only once&lt;BR /&gt;mfw_gst_audio_pp.c:408: error: for each function it appears in.)&lt;BR /&gt;mfw_gst_audio_pp.c:408: error: 'ppl' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:411: error: 'PEQ_INSTANCE_CONTEXT' has no member named 'peqpl'&lt;BR /&gt;mfw_gst_audio_pp.c:416: error: 'PEQ_I32' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:416: error: expected expression before ')' token&lt;BR /&gt;mfw_gst_audio_pp.c:420: error: expected expression before ')' token&lt;BR /&gt;mfw_gst_audio_pp.c: In function 'parametric_eq_do_process':&lt;BR /&gt;mfw_gst_audio_pp.c:433: error: 'PEQ_PL' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:433: error: 'ppl' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:433: error: 'PEQ_INSTANCE_CONTEXT' has no member named 'peqpl'&lt;BR /&gt;mfw_gst_audio_pp.c:434: error: 'PEQ_PPP_Config' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:434: error: 'ppconfig' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:434: error: 'PEQ_INSTANCE_CONTEXT' has no member named 'peqconfig'&lt;BR /&gt;mfw_gst_audio_pp.c:435: error: 'PEQ_INFO' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:435: error: 'ppinfo' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:435: error: 'PEQ_INSTANCE_CONTEXT' has no member named 'pqeinfo'&lt;BR /&gt;mfw_gst_audio_pp.c: In function 'parametric_eq_instancelize':&lt;BR /&gt;mfw_gst_audio_pp.c:450: error: 'PEQ_PPP_Config' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:450: error: 'pconfig' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:451: error: 'PEQ_PL' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:451: error: 'ppl' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:452: error: 'PEQ_Mem_Alloc_Info_Sub' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:452: error: 'mem_sub' undeclared (first use in this function)&lt;BR /&gt;mfw_gst_audio_pp.c:469: error: 'PEQ_INSTANCE_CONTEXT' has no member named 'peqconfig'&lt;BR /&gt;mfw_gst_audio_pp.c:485: error: 'PEQ_INSTANCE_CONTEXT' has no member named 'peqpl'&lt;BR /&gt;mfw_gst_audio_pp.c:504: error: 'PEQ_INSTANCE_CONTEXT' has no member named 'peqconfig'&lt;BR /&gt;mfw_gst_audio_pp.c: In function 'mfw_gst_audio_pp_init':&lt;BR /&gt;mfw_gst_audio_pp.c:767: warning: format '%s' expects type 'char *', but argument 2 has type 'int'&lt;BR /&gt;make[1]: *** [libmfw_gst_audio_pp_la-mfw_gst_audio_pp.lo] Error 1&lt;BR /&gt;make[1]: Leaving directory `/home/abc/imx53/11.09.01/L2.6.35_11.09.01_ER_source/LTIB/ltib/rpm/BUILD/gst-fsl-plugin-2.0.3/src/audio/audio_pp/src'&lt;BR /&gt;make: *** [all-recursive] Error 1&lt;BR /&gt;error: Bad exit status from /home/abc/imx53/11.09.01/L2.6.35_11.09.01_ER_source/LTIB/ltib/tmp/rpm-tmp.1179 (%build)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;RPM build errors:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bad exit status from /home/abc/imx53/11.09.01/L2.6.35_11.09.01_ER_source/LTIB/ltib/tmp/rpm-tmp.1179 (%build)&lt;BR /&gt;Build time for gst-fsl-plugin: 16 seconds&lt;/P&gt;&lt;P&gt;Failed building gst-fsl-plugin&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;f_buildrpms() returned an error, exiting&lt;BR /&gt;traceback:&lt;BR /&gt; main:560&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Started: Mon Oct&amp;nbsp; 8 15:54:40 2012&lt;BR /&gt;Ended:&amp;nbsp;&amp;nbsp; Mon Oct&amp;nbsp; 8 15:55:53 2012&lt;BR /&gt;Elapsed: 73 seconds&lt;/P&gt;&lt;P&gt;These packages failed to build:&lt;BR /&gt;gst-fsl-plugin&lt;/P&gt;&lt;P&gt;Build Failed&lt;/P&gt;&lt;P&gt;Exiting on error or interrupt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did checked the directory "`/home/abc/imx53/11.09.01/L2.6.35_11.09.01_ER_source/LTIB/ltib&lt;STRONG&gt;/rpm/BUILD/gst-fsl-plugin-2.0.3/src/audio/audio_pp/src&lt;/STRONG&gt;" and there is no such file as "&lt;STRONG&gt;peq_ppp_interface.h&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would appreciate if any inputs to resolve the issue are provided.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2012 10:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gst-fsl-plugin-build-failed/m-p/210943#M12667</guid>
      <dc:creator>AjayKaushik</dc:creator>
      <dc:date>2012-10-08T10:32:53Z</dc:date>
    </item>
    <item>
      <title>Re: gst-fsl-plugin build failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gst-fsl-plugin-build-failed/m-p/210944#M12668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The &lt;STRONG&gt;peq_ppp_interface.h &lt;/STRONG&gt;is not in the same directory as the plugins, but is located in codec package fsl-mm-codeclib-2.0.3-2.tar.gz (fsl-mm-codeclib-2.0.3\ghdr\). you can check if it is existent in the codec package.&lt;/P&gt;&lt;P&gt;Please start with a clean build.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2012 06:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gst-fsl-plugin-build-failed/m-p/210944#M12668</guid>
      <dc:creator>PhilChen</dc:creator>
      <dc:date>2012-10-09T06:53:57Z</dc:date>
    </item>
  </channel>
</rss>