<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6-yocto-automake:- failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-yocto-automake-failed/m-p/823367#M126653</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kalaiyarasan Selvaraj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which BSP are you using? The training uses the Dora branch, which was released in October 2013. I would recommend using a newer branch. You can find the latest branches of the Community BSP on the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://freescale.github.io/"&gt;http://freescale.github.io/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also make sure you install the corresponding version of the packages required for the Ubuntu host:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.yoctoproject.org/docs/latest/ref-manual/ref-manual.html#ubuntu-packages"&gt;https://www.yoctoproject.org/docs/latest/ref-manual/ref-manual.html#ubuntu-packages&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Dec 2018 21:24:06 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-12-05T21:24:06Z</dc:date>
    <item>
      <title>imx6-yocto-automake:- failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-yocto-automake-failed/m-p/823366#M126652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/docs/DOC-94914#comments" title="https://community.nxp.com/docs/DOC-94914#comments"&gt;Hi,&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I start learning yocto build for imx 6. I followed the link &lt;A href="https://community.nxp.com/docs/DOC-94849"&gt;Yocto Training - HOME&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;during my first build, &lt;A href="https://community.nxp.com/docs/DOC-94914"&gt;Task #2 - First build&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; automake get failed, I am using ubuntu 16.04.&lt;/P&gt;&lt;P&gt;why x86_64 is being build?&lt;/P&gt;&lt;P&gt;how can i resolve this, It look like not direct?&amp;nbsp;&amp;nbsp;&amp;nbsp; I have gone to automake bb file. i could not find any do_compile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have given my error print below:-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Preparing runqueue&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: Function failed: do_compile (log file is located at /media/adminx/linux/nxp_yocto/fsl-community-bsp/build/tmp/work/x86_64-linux/automake-native/1.12.6-r0/temp/log.do_compile.9678)&lt;BR /&gt;ERROR: Logfile of failure stored in: /media/adminx/linux/nxp_yocto/fsl-community-bsp/build/tmp/work/x86_64-linux/automake-native/1.12.6-r0/temp/log.do_compile.9678&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_compile&lt;BR /&gt;| NOTE: make -j 4&lt;BR /&gt;| : &amp;amp;&amp;amp; /bin/mkdir -p doc &amp;amp;&amp;amp; PATH="/media/adminx/linux/nxp_yocto/fsl-community-bsp/build/tmp/work/x86_64-linux/automake-native/1.12.6-r0/build/t/wrap:$PATH" &amp;amp;&amp;amp; export PATH &amp;amp;&amp;amp; /usr/bin/perl /media/adminx/linux/nxp_yocto/fsl-community-bsp/build/tmp/work/x86_64-linux/automake-native/1.12.6-r0/automake-1.12.6/doc/help2man --output=doc/automake-1.12.1 automake-1.12&lt;BR /&gt;| help2man: can't get `--help' info from automake-1.12&lt;BR /&gt;| Try `--no-discard-stderr' if option outputs to stderr&lt;BR /&gt;| Makefile:4114: recipe for target 'doc/automake-1.12.1' failed&lt;BR /&gt;| make: *** [doc/automake-1.12.1] Error 255&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /media/adminx/linux/nxp_yocto/fsl-community-bsp/build/tmp/work/x86_64-linux/automake-native/1.12.6-r0/temp/log.do_compile.9678)&lt;BR /&gt;ERROR: Task 421 (virtual:native:/media/adminx/linux/nxp_yocto/fsl-community-bsp/sources/poky/meta/recipes-devtools/automake/automake_1.12.6.bb, do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 119 tasks of which 113 didn't need to be rerun and 1 failed.&lt;BR /&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt; virtual:native:/media/adminx/linux/nxp_yocto/fsl-community-bsp/sources/poky/meta/recipes-devtools/automake/automake_1.12.6.bb, do_compile&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/space/2004"&gt;i.MX Processors&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2018 16:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-yocto-automake-failed/m-p/823366#M126652</guid>
      <dc:creator>kalaiyarasansel</dc:creator>
      <dc:date>2018-11-30T16:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx6-yocto-automake:- failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-yocto-automake-failed/m-p/823367#M126653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kalaiyarasan Selvaraj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which BSP are you using? The training uses the Dora branch, which was released in October 2013. I would recommend using a newer branch. You can find the latest branches of the Community BSP on the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://freescale.github.io/"&gt;http://freescale.github.io/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also make sure you install the corresponding version of the packages required for the Ubuntu host:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.yoctoproject.org/docs/latest/ref-manual/ref-manual.html#ubuntu-packages"&gt;https://www.yoctoproject.org/docs/latest/ref-manual/ref-manual.html#ubuntu-packages&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2018 21:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-yocto-automake-failed/m-p/823367#M126653</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-12-05T21:24:06Z</dc:date>
    </item>
  </channel>
</rss>