<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to implement the V4l2 camera control in IMX8M</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-implement-the-V4l2-camera-control-in-IMX8M/m-p/823280#M126649</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Reshvanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check linux/drivers/media/platform/imx8&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/imx8?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/imx8?h=imx_4.14.78_1.0.0_ga"&gt;imx8\platform\media\drivers - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and sect.6.1.4 MIPI Camera Serial Interface (MIPI CSI) attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Dec 2018 01:21:56 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-12-24T01:21:56Z</dc:date>
    <item>
      <title>How to implement the V4l2 camera control in IMX8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-implement-the-V4l2-camera-control-in-IMX8M/m-p/823279#M126648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;I am using the ROCKO distribution of yacto bsp for IMX8M EVK board with default OV5640 camera. I can able to stream the camera with the default ov5640_mipi-v2.ko driver but the default driver does not support the V4L2 camera controls(like brightness, exposure) so i followed this link &lt;A class="" href="https://linuxtv.org/downloads/v4l-dvb-apis/kapi/v4l2-controls.html" title="https://linuxtv.org/downloads/v4l-dvb-apis/kapi/v4l2-controls.html"&gt;1.12. V4L2 Controls — Linux Media Subsystem Documentation documentation&lt;/A&gt;&amp;nbsp; and implement the controls. The implemented controls are registered without any error but when i tried to list the supported controls using "v4l2-ctl --list-ctrls" it does not display any controls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i tried to set the brightness by using "v4l2-ctl -c brightness=2" it shows unknown control. Is there any sample code or document available means, its really helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards&lt;/P&gt;&lt;P&gt;Reshvanth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Dec 2018 06:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-implement-the-V4l2-camera-control-in-IMX8M/m-p/823279#M126648</guid>
      <dc:creator>reshwanth_r</dc:creator>
      <dc:date>2018-12-21T06:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: How to implement the V4l2 camera control in IMX8M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-implement-the-V4l2-camera-control-in-IMX8M/m-p/823280#M126649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Reshvanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check linux/drivers/media/platform/imx8&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/imx8?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/media/platform/imx8?h=imx_4.14.78_1.0.0_ga"&gt;imx8\platform\media\drivers - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and sect.6.1.4 MIPI Camera Serial Interface (MIPI CSI) attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Dec 2018 01:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-implement-the-V4l2-camera-control-in-IMX8M/m-p/823280#M126649</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-24T01:21:56Z</dc:date>
    </item>
  </channel>
</rss>