<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Audio Capabilities of i.MX6UL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Capabilities-of-i-MX6UL/m-p/823134#M126637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aquiel Godeau,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see on the i.MX6UL datasheet (link below) that this processor has a SAI module which provides a synchronous audio interface (SAI) that supports full duplex serial interfaces with frame synchronization, such as I2S, AC97, TDM, and codec/DSP interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fdata-sheet%2FIMX6ULCEC.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that while it does have audio capabilities you would need to add a codec to which you can connect an audio jack or a speaker (with amplification if desired).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see the i.MX6UL EVK for an example of how audio is implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Dec 2018 22:58:24 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-12-21T22:58:24Z</dc:date>
    <item>
      <title>Audio Capabilities of i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Capabilities-of-i-MX6UL/m-p/823133#M126636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I was wondering if the i.MX6UL&amp;nbsp;has any audio capabilities, it is not clear from the documentation I have. I am looking to implement a speaker and need to know if I need an additional IC.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Dec 2018 22:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-Capabilities-of-i-MX6UL/m-p/823133#M126636</guid>
      <dc:creator>agodeau</dc:creator>
      <dc:date>2018-12-20T22:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: Audio Capabilities of i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Capabilities-of-i-MX6UL/m-p/823134#M126637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aquiel Godeau,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see on the i.MX6UL datasheet (link below) that this processor has a SAI module which provides a synchronous audio interface (SAI) that supports full duplex serial interfaces with frame synchronization, such as I2S, AC97, TDM, and codec/DSP interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fdata-sheet%2FIMX6ULCEC.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that while it does have audio capabilities you would need to add a codec to which you can connect an audio jack or a speaker (with amplification if desired).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see the i.MX6UL EVK for an example of how audio is implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Dec 2018 22:58:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-Capabilities-of-i-MX6UL/m-p/823134#M126637</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-12-21T22:58:24Z</dc:date>
    </item>
    <item>
      <title>Re: Audio Capabilities of i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Capabilities-of-i-MX6UL/m-p/823135#M126638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using MYIR's &lt;A href="http://www.myirtech.com/list.asp?id=573"&gt;MYD-Y6ULX development board&lt;/A&gt;. The audio is brought out through I2S.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="audio.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71561iE21153A34D1FB948/image-size/large?v=v2&amp;amp;px=999" role="button" title="audio.png" alt="audio.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2019 08:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-Capabilities-of-i-MX6UL/m-p/823135#M126638</guid>
      <dc:creator>linda_zhang</dc:creator>
      <dc:date>2019-01-04T08:33:45Z</dc:date>
    </item>
  </channel>
</rss>