<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.mx6ul kernel hangs on key type dns_resolver registered</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ul-kernel-hangs-on-key-type-dns-resolver-registered/m-p/822755#M126581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just try to disable the FEC driver in the kernel menuconfig as per the Chapter 43 of the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Sep 2018 10:54:35 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2018-09-19T10:54:35Z</dc:date>
    <item>
      <title>i.mx6ul kernel hangs on key type dns_resolver registered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ul-kernel-hangs-on-key-type-dns-resolver-registered/m-p/822754#M126580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Boot log follows. I've made a lot of progress on my custom board. It was hanging on crypto caam so i disabled everthing with crypto caam in imx_v7_defconfig but now it's hanging on this dns thing.&amp;nbsp; I think I need to somehow disable the hardwired ethernet port because i'm not using the ethernet controllers on this processor (i will be using bt/wifi through uart/sdio later, but not the ethernet peripherals).&amp;nbsp; if i should be disabling ethernet in the kernel, how do i do that? otherwise, how do i get past it hanging on this dns thing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boot log:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;U-Boot 2016.03 (Sep 13 2018 - 14:46:49 -0400)&lt;BR /&gt;arm-linux-gnueabihf-gcc (Linaro GCC 7.2-2017.11) 7.2.1 20171011&lt;BR /&gt;GNU ld (Linaro_Binutils-2017.11) 2.28.2.20170706&lt;BR /&gt;=&amp;gt; run bootcmd&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;reading boot.scr&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;reading zImage&lt;BR /&gt;6643144 bytes read in 299 ms (21.2 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;reading imx6ul-14x14-evk.dtb&lt;BR /&gt;36350 bytes read in 20 ms (1.7 MiB/s)&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x655dc8 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt; Booting using the fdt blob at 0x83000000&lt;BR /&gt; Using Device Tree in place at 83000000, end 8300bdfd&lt;BR /&gt;Modify /soc/aips-bus@02000000/bee@02044000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.1.15 (user@dave-VBOX-UBUNTU) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11) ) #10 SMP PREEMPT Thu Sep 13 14:29:52 EDT 2018&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;BR /&gt;Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB&lt;BR /&gt;Reserved memory: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;PERCPU: Embedded 12 pages/cpu @8bb32000 s16908 r8192 d24052 u49152&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw&lt;BR /&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;Memory: 178712K/524288K available (8296K kernel code, 428K rwdata, 2912K rodata, 436K init, 450K bss, 17896K reserved, 327680K cma-reserved, 0K highmem)&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xffc00000 - 0xfff00000 (3072 kB)&lt;BR /&gt; vmalloc : 0xa0800000 - 0xff000000 (1512 MB)&lt;BR /&gt; lowmem : 0x80000000 - 0xa0000000 ( 512 MB)&lt;BR /&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;BR /&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;BR /&gt; .text : 0x80008000 - 0x80afa2f8 (11209 kB)&lt;BR /&gt; .init : 0x80afb000 - 0x80b68000 ( 436 kB)&lt;BR /&gt; .data : 0x80b68000 - 0x80bd3380 ( 429 kB)&lt;BR /&gt; .bss : 0x80bd6000 - 0x80c46800 ( 450 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt; Additional per-CPU info printed with stalls.&lt;BR /&gt; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.&lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;mxc_clocksource_init 3000000&lt;BR /&gt;Switching to timer-based delay loop, resolution 333ns&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns&lt;BR /&gt;clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;/cpus/cpu@0 missing clock-frequency property&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x80008280 - 0x800082d8&lt;BR /&gt;Brought up 1 CPUs&lt;BR /&gt;SMP: Total of 1 processors activated (6.00 BogoMIPS).&lt;BR /&gt;CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;devtmpfs: initialized&lt;BR /&gt;device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;BR /&gt;clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns&lt;BR /&gt;pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;BR /&gt;cpuidle: using governor ladder&lt;BR /&gt;cpuidle: using governor menu&lt;BR /&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;BR /&gt;imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;BR /&gt;mxs-dma 1804000.dma-apbh: initialized&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;i2c i2c-0: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-0: can't use DMA&lt;BR /&gt;i2c i2c-1: IMX I2C adapter registered&lt;BR /&gt;i2c i2c-1: can't use DMA&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;PTP clock support registered&lt;BR /&gt;MIPI CSI2 driver module loaded&lt;BR /&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;Bluetooth: Core ver 2.20&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;Switched to clocksource mxc_timer1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;TCP established hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;TCP bind hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 4096 bind 4096)&lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;imx rpmsg driver is registered.&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;futex hash table entries: 256 (order: 2, 16384 bytes)&lt;BR /&gt;VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;NFS: Registering the id_resolver key type&lt;BR /&gt;Key type id_resolver registered&lt;BR /&gt;Key type id_legacy registered&lt;BR /&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.23)&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;imx-weim 21b8000.weim: Driver registered.&lt;BR /&gt;backlight supply power not found, using dummy regulator&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;21c8000.lcdif supply lcd not found, using dummy regulator&lt;BR /&gt;mxsfb 21c8000.lcdif: failed to find mxc display driver&lt;BR /&gt;Console: switching to colour frame buffer device 100x30&lt;BR /&gt;mxsfb 21c8000.lcdif: initialized&lt;BR /&gt;imx-sdma 20ec000.sdma: no event needs to be remapped&lt;BR /&gt;imx-sdma 20ec000.sdma: loaded firmware 3.3&lt;BR /&gt;imx-sdma 20ec000.sdma: initialized&lt;BR /&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX&lt;BR /&gt;console [ttymxc0] enabled&lt;BR /&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX&lt;BR /&gt;imx sema4 driver is registered.&lt;BR /&gt;[drm] Initialized drm 1.1.0 20060810&lt;BR /&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0&lt;BR /&gt;brd: module loaded&lt;BR /&gt;loop: module loaded&lt;BR /&gt;fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff&lt;BR /&gt;fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed&lt;BR /&gt;spi_gpio spi4: gpio-miso property not found, switching to no-rx mode&lt;BR /&gt;CAN device driver interface&lt;BR /&gt;flexcan 2090000.can: device registered (reg_base=a09e8000, irq=28)&lt;BR /&gt;flexcan 2094000.can: device registered (reg_base=a09f0000, irq=29)&lt;BR /&gt;20b4000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps0: new PPS source ptp0&lt;BR /&gt;fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: a2:ae:ae:c3:3f:4d&lt;BR /&gt;libphy: fec_enet_mii_bus: probed&lt;BR /&gt;fec 20b4000.ethernet eth0: registered PHC device 0&lt;BR /&gt;2188000.ethernet supply phy not found, using dummy regulator&lt;BR /&gt;pps pps1: new PPS source ptp1&lt;BR /&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00&lt;BR /&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: c6:f5:cf:dd:0e:58&lt;BR /&gt;fec 2188000.ethernet eth1: registered PHC device 1&lt;BR /&gt;usbcore: registered new interface driver asix&lt;BR /&gt;usbcore: registered new interface driver ax88179_178a&lt;BR /&gt;usbcore: registered new interface driver cdc_ether&lt;BR /&gt;usbcore: registered new interface driver net1080&lt;BR /&gt;usbcore: registered new interface driver cdc_subset&lt;BR /&gt;usbcore: registered new interface driver zaurus&lt;BR /&gt;usbcore: registered new interface driver cdc_ncm&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;ehci-mxc: Freescale On-Chip EHCI Host driver&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;usbcore: registered new interface driver usb_ehset_test&lt;BR /&gt;2184800.usbmisc supply vbus-wakeup not found, using dummy regulator&lt;BR /&gt;2184000.usb supply vbus not found, using dummy regulator&lt;BR /&gt;2184200.usb supply vbus not found, using dummy regulator&lt;BR /&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller&lt;BR /&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1&lt;BR /&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0&lt;BR /&gt;input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1&lt;BR /&gt;input: TSC2007 Touchscreen as /devices/platform/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-0049/input/input2&lt;BR /&gt;read sensor who am i (0xfffffffb)error !&lt;BR /&gt;fxls8471: probe of 0-001e failed with error -22&lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;IR NEC protocol handler initialized&lt;BR /&gt;IR RC5(x/sz) protocol handler initialized&lt;BR /&gt;IR RC6 protocol handler initialized&lt;BR /&gt;IR JVC protocol handler initialized&lt;BR /&gt;IR Sony protocol handler initialized&lt;BR /&gt;IR SANYO protocol handler initialized&lt;BR /&gt;IR Sharp protocol handler initialized&lt;BR /&gt;IR MCE Keyboard/mouse protocol handler initialized&lt;BR /&gt;IR XMP protocol handler initialized&lt;BR /&gt;pxp-v4l2 pxp_v4l2: initialized&lt;BR /&gt;0-000e supply vdd not found, using dummy regulator&lt;BR /&gt;0-000e supply vddio not found, using dummy regulator&lt;BR /&gt;mag3110 0-000e: check mag3110 chip ID&lt;BR /&gt;mag3110 0-000e: read chip ID 0xfffffffb is not equal to 0xc4!&lt;BR /&gt;mag3110: probe of 0-000e failed with error -22&lt;BR /&gt;imx2-wdt 20bc000.wdog: use WDOG_B to reboot.&lt;BR /&gt;imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)&lt;BR /&gt;Bluetooth: HCI UART driver ver 2.3&lt;BR /&gt;Bluetooth: HCI UART protocol H4 registered&lt;BR /&gt;Bluetooth: HCI UART protocol BCSP registered&lt;BR /&gt;Bluetooth: HCI UART protocol ATH3K registered&lt;BR /&gt;usbcore: registered new interface driver bcm203x&lt;BR /&gt;usbcore: registered new interface driver btusb&lt;BR /&gt;usbcore: registered new interface driver ath3k&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO&lt;BR /&gt;sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA&lt;BR /&gt;/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found&lt;BR /&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;wm8960 1-001a: Failed to issue reset&lt;BR /&gt;wm8960: probe of 1-001a failed with error -11&lt;BR /&gt;fsl-asrc 2034000.asrc: driver registered&lt;BR /&gt;imx-wm8960 sound: failed to find codec platform device&lt;BR /&gt;imx-wm8960: probe of sound failed with error -22&lt;BR /&gt;NET: Registered protocol family 26&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;sit: IPv6 over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;can: controller area network core (rev 20120528 abi 9)&lt;BR /&gt;NET: Registered protocol family 29&lt;BR /&gt;can: raw protocol (rev 20120528)&lt;BR /&gt;can: broadcast manager protocol (rev 20120528 t)&lt;BR /&gt;can: netlink gateway (rev 20130117) max_hops=1&lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;Bluetooth: BNEP socket layer initialized&lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;Bluetooth: HIDP socket layer initialized&lt;BR /&gt;8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;Key type dns_resolver registered&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 18:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6ul-kernel-hangs-on-key-type-dns-resolver-registered/m-p/822754#M126580</guid>
      <dc:creator>dluberger</dc:creator>
      <dc:date>2018-09-13T18:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6ul kernel hangs on key type dns_resolver registered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ul-kernel-hangs-on-key-type-dns-resolver-registered/m-p/822755#M126581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just try to disable the FEC driver in the kernel menuconfig as per the Chapter 43 of the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2018 10:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6ul-kernel-hangs-on-key-type-dns-resolver-registered/m-p/822755#M126581</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-09-19T10:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6ul kernel hangs on key type dns_resolver registered</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ul-kernel-hangs-on-key-type-dns-resolver-registered/m-p/822756#M126582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This looks a lot like a hang I was seeing. Try this patch&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/commit/516eef7e45003969d538e89f339c73c6c1133cbe" title="https://github.com/boundarydevices/linux-imx6/commit/516eef7e45003969d538e89f339c73c6c1133cbe"&gt;mach-imx6ul: use syscon_node_to_regmap to get grading · boundarydevices/linux-imx6@516eef7 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2020 01:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6ul-kernel-hangs-on-key-type-dns-resolver-registered/m-p/822756#M126582</guid>
      <dc:creator>TroyKisky</dc:creator>
      <dc:date>2020-02-05T01:20:47Z</dc:date>
    </item>
  </channel>
</rss>