<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSPI read problem on iMX6.UL (no MISO data)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-read-problem-on-iMX6-UL-no-MISO-data/m-p/822532#M126563</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone&amp;nbsp;had (and ideally solved!) problems with SPI master on the UL?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;I’m using a 4.4.40 kernel, and&amp;nbsp;&lt;/SPAN&gt;trying a simple loopback test (MOSI shorted to MISO) with the spi_imx driver module and “spidev_test” utility.&lt;/P&gt;&lt;P&gt;I also have a bus analyser hooked up and this sees the data on MISO as well as MOSI, but the utility just gets zeroes back.&lt;/P&gt;&lt;P&gt;My board uses an SOM and I can swap the UL for a iMX6.S and it works – so I know there isn’t a wiring fault on the board. I don't think there's any significant difference in kernel config (though obviously the device trees are quite different).&lt;/P&gt;&lt;P&gt;I feel the device tree is &lt;EM&gt;probably&lt;/EM&gt; correct, because Clk/SS/MOSI are all working; just not MISO. I have my own top-level dts for my board, but it includes the imx6ul-tx6ul.dtsi and&amp;nbsp;imx6ul.dtsi from the kernel source.&lt;/P&gt;&lt;P&gt;Any thoughts please as to where the problem could be? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 25 Aug 2018 15:14:44 GMT</pubDate>
    <dc:creator>colinhelliwell</dc:creator>
    <dc:date>2018-08-25T15:14:44Z</dc:date>
    <item>
      <title>SPI read problem on iMX6.UL (no MISO data)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-read-problem-on-iMX6-UL-no-MISO-data/m-p/822532#M126563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone&amp;nbsp;had (and ideally solved!) problems with SPI master on the UL?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;I’m using a 4.4.40 kernel, and&amp;nbsp;&lt;/SPAN&gt;trying a simple loopback test (MOSI shorted to MISO) with the spi_imx driver module and “spidev_test” utility.&lt;/P&gt;&lt;P&gt;I also have a bus analyser hooked up and this sees the data on MISO as well as MOSI, but the utility just gets zeroes back.&lt;/P&gt;&lt;P&gt;My board uses an SOM and I can swap the UL for a iMX6.S and it works – so I know there isn’t a wiring fault on the board. I don't think there's any significant difference in kernel config (though obviously the device trees are quite different).&lt;/P&gt;&lt;P&gt;I feel the device tree is &lt;EM&gt;probably&lt;/EM&gt; correct, because Clk/SS/MOSI are all working; just not MISO. I have my own top-level dts for my board, but it includes the imx6ul-tx6ul.dtsi and&amp;nbsp;imx6ul.dtsi from the kernel source.&lt;/P&gt;&lt;P&gt;Any thoughts please as to where the problem could be? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Aug 2018 15:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-read-problem-on-iMX6-UL-no-MISO-data/m-p/822532#M126563</guid>
      <dc:creator>colinhelliwell</dc:creator>
      <dc:date>2018-08-25T15:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: SPI read problem on iMX6.UL (no MISO data)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-read-problem-on-iMX6-UL-no-MISO-data/m-p/822533#M126564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi colinhelliwell&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;4.4.40 kernel is not supported by nxp, one can try with official nxp releases described on &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;below example dts from L4.1.15 kernel,&amp;nbsp; linux/arch/arm/boot/dts/imx6ul-14x14-evk.dts&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk.dts?h=imx_4.1.15_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk.dts?h=imx_4.1.15_2.0.0_ga"&gt;imx6ul-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Aug 2018 23:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-read-problem-on-iMX6-UL-no-MISO-data/m-p/822533#M126564</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-26T23:06:24Z</dc:date>
    </item>
  </channel>
</rss>