<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX6 uboot fuse command</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-fuse-command/m-p/822092#M126547</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 浩 刘&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fuses may be locked, please check Table Lock Fuses in Chapter &lt;BR /&gt;Fusemap Reference Manual processor which are you using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jul 2018 23:10:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-07-17T23:10:16Z</dc:date>
    <item>
      <title>IMX6 uboot fuse command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-fuse-command/m-p/822091#M126546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want write some value to fuse&lt;/P&gt;&lt;P&gt;In uboot I try "fuse prog 3 0 xxxx"&lt;/P&gt;&lt;P&gt;And then I use "fuse read 3 0", out put 0&lt;/P&gt;&lt;P&gt;It seem &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;the command did not take effect&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Before I need to use "fuse prog 3 0" , Any pre-operation such as the need to do other bits to be rewritten?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 14:06:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-fuse-command/m-p/822091#M126546</guid>
      <dc:creator>liuhao1</dc:creator>
      <dc:date>2018-07-17T14:06:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 uboot fuse command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-fuse-command/m-p/822092#M126547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 浩 刘&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fuses may be locked, please check Table Lock Fuses in Chapter &lt;BR /&gt;Fusemap Reference Manual processor which are you using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 23:10:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-uboot-fuse-command/m-p/822092#M126547</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-17T23:10:16Z</dc:date>
    </item>
  </channel>
</rss>