<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Which gstreamer package do I need to bitbake if I want to let my Qmediaplayer work in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Which-gstreamer-package-do-I-need-to-bitbake-if-I-want-to-let-my/m-p/820980#M126411</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I'm working on i.MX6 Quad sabre-SD and utilize freescale release yocto project to build weston wayland as my OS system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I designed a QT application that could play video via Qmediaplayer.&lt;/P&gt;&lt;P&gt;But I found out that I do not have any player to play.&lt;/P&gt;&lt;P&gt;So I tried to build gstreamer for my root file system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is what I got all the receipt that I could bitbake.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;packagegroup-fsl-gstreamer1.0 :1.0-r0&lt;BR /&gt;packagegroup-fsl-gstreamer1.0-full :1.0-r0&lt;/P&gt;&lt;P&gt;packagegroup-fsl-multimedia-gstreamer1.0-core :1.0-r0&lt;BR /&gt;packagegroup-fsl-multimedia-gstreamer1.0-testapps :1.0-r0&lt;/P&gt;&lt;P&gt;gstreamer :0.10.36-r2&lt;BR /&gt;gstreamer1.0 :1.6.0-r0&lt;BR /&gt;gstreamer1.0-meta-base :1.0-r0&lt;BR /&gt;gstreamer1.0-plugins-bad :1.6.0-r0&lt;BR /&gt;gstreamer1.0-plugins-base :1.6.0-r0&lt;BR /&gt;gstreamer1.0-plugins-good :1.6.0-r0&lt;BR /&gt;gstreamer1.0-plugins-imx :0.12.0-r0&lt;BR /&gt;gstreamer1.0-rtsp-server :1.6.0-r0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which one should I build?&lt;/P&gt;&lt;P&gt;And what is difference between them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is there any method that I could add something in bb file and bitbake fsl-image-qt5 then it will include all the mediaplayer into root file system?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Moreover, is there any menuconfig that I should set to proper fit media player?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advanced!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Oct 2018 08:27:41 GMT</pubDate>
    <dc:creator>wangtsungli</dc:creator>
    <dc:date>2018-10-23T08:27:41Z</dc:date>
    <item>
      <title>Which gstreamer package do I need to bitbake if I want to let my Qmediaplayer work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-gstreamer-package-do-I-need-to-bitbake-if-I-want-to-let-my/m-p/820980#M126411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I'm working on i.MX6 Quad sabre-SD and utilize freescale release yocto project to build weston wayland as my OS system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I designed a QT application that could play video via Qmediaplayer.&lt;/P&gt;&lt;P&gt;But I found out that I do not have any player to play.&lt;/P&gt;&lt;P&gt;So I tried to build gstreamer for my root file system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is what I got all the receipt that I could bitbake.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;packagegroup-fsl-gstreamer1.0 :1.0-r0&lt;BR /&gt;packagegroup-fsl-gstreamer1.0-full :1.0-r0&lt;/P&gt;&lt;P&gt;packagegroup-fsl-multimedia-gstreamer1.0-core :1.0-r0&lt;BR /&gt;packagegroup-fsl-multimedia-gstreamer1.0-testapps :1.0-r0&lt;/P&gt;&lt;P&gt;gstreamer :0.10.36-r2&lt;BR /&gt;gstreamer1.0 :1.6.0-r0&lt;BR /&gt;gstreamer1.0-meta-base :1.0-r0&lt;BR /&gt;gstreamer1.0-plugins-bad :1.6.0-r0&lt;BR /&gt;gstreamer1.0-plugins-base :1.6.0-r0&lt;BR /&gt;gstreamer1.0-plugins-good :1.6.0-r0&lt;BR /&gt;gstreamer1.0-plugins-imx :0.12.0-r0&lt;BR /&gt;gstreamer1.0-rtsp-server :1.6.0-r0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which one should I build?&lt;/P&gt;&lt;P&gt;And what is difference between them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is there any method that I could add something in bb file and bitbake fsl-image-qt5 then it will include all the mediaplayer into root file system?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Moreover, is there any menuconfig that I should set to proper fit media player?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advanced!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 08:27:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-gstreamer-package-do-I-need-to-bitbake-if-I-want-to-let-my/m-p/820980#M126411</guid>
      <dc:creator>wangtsungli</dc:creator>
      <dc:date>2018-10-23T08:27:41Z</dc:date>
    </item>
    <item>
      <title>Re: Which gstreamer package do I need to bitbake if I want to let my Qmediaplayer work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Which-gstreamer-package-do-I-need-to-bitbake-if-I-want-to-let-my/m-p/820981#M126412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved the problem to add this line in my conf/local.conf&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;PACKAGECONFIG_append_pn-qtmultimedia = " gstreamer"&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This will auto build all the relevant gstreamer and build rootfs out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After add this line, I should execute bitbake fsl-image-qt5 to build rootfs again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 10:11:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Which-gstreamer-package-do-I-need-to-bitbake-if-I-want-to-let-my/m-p/820981#M126412</guid>
      <dc:creator>wangtsungli</dc:creator>
      <dc:date>2018-10-23T10:11:43Z</dc:date>
    </item>
  </channel>
</rss>