<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic u-boot standalone application in sabre SD board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820204#M126307</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.,.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on imx6 dual lite sabre SD board(free scale board), In this i managed to compile u-boot image and boot it from SD card(SD card slot3), my requirement is to run a standalone example from SD card, I tried by copying hello_world .bin(which is already been compiled with u-boot) file to fat partition of SD card and tried to load by using fatload command, but it was showing&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;BR /&gt;** Bad device mmc ** &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions or some references would be appreciated&amp;nbsp; lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Aug 2018 09:35:45 GMT</pubDate>
    <dc:creator>karthikas</dc:creator>
    <dc:date>2018-08-23T09:35:45Z</dc:date>
    <item>
      <title>u-boot standalone application in sabre SD board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820204#M126307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.,.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on imx6 dual lite sabre SD board(free scale board), In this i managed to compile u-boot image and boot it from SD card(SD card slot3), my requirement is to run a standalone example from SD card, I tried by copying hello_world .bin(which is already been compiled with u-boot) file to fat partition of SD card and tried to load by using fatload command, but it was showing&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;BR /&gt;** Bad device mmc ** &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions or some references would be appreciated&amp;nbsp; lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 09:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820204#M126307</guid>
      <dc:creator>karthikas</dc:creator>
      <dc:date>2018-08-23T09:35:45Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot standalone application in sabre SD board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820205#M126308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi karthik,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could modified the mmc block 0:1 or 1:1. Example: fatload mmc 1:1 0x00907000&lt;/P&gt;&lt;P&gt;It works when I performed the ddr stress test in uboot, hope it works, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 01:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820205#M126308</guid>
      <dc:creator>nxf45220</dc:creator>
      <dc:date>2018-08-27T01:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot standalone application in sabre SD board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820206#M126309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai.,.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes you are correct, after changing to mmc 1:1 it was loading into RAM successfully , Now if I give go command its throwing a data abort error and also board is getting Reset. Any Idea what could be the issue,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running standalone program without modifying single line&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the log&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;=&amp;gt; &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;=&amp;gt; fatload mmc 1:2 0x12000000 hello_world.bin&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;578 bytes read in 13 ms (43 KiB/s)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;=&amp;gt; &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;=&amp;gt; go 0x12000000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;## Starting application at 0x12000000 ...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;data abort&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;pc : [&amp;lt;12000008&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lr : [&amp;lt;4ff683d7&amp;gt;]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;reloc pc : [&amp;lt;d989b008&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; lr : [&amp;lt;178033d7&amp;gt;]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;sp : 4f564d48&amp;nbsp; ip : 0000001c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fp : 00000002&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;r10: 4ffc436c&amp;nbsp; r9 : 4f564ea8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r8 : 4f567938&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;r7 : 4ff683ad&amp;nbsp; r6 : 00000002&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r5 : 12000000&amp;nbsp; r4 : 4f56793c&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;r3 : 12000000&amp;nbsp; r2 : 4f56793c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1 : 4f56793c&amp;nbsp; r0 : 00000001&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Flags: nzCv&amp;nbsp; IRQs off&amp;nbsp; FIQs off&amp;nbsp; Mode SVC_32&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Code: e4df8df7 cedfb73f 41f0e92d 46084605 (2400460e) &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Resetting CPU ...&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;resetting ...&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot SPL 2018.07-rc2-dirty (Aug 24 2018 - 10:03:53 +0530)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Trying to boot from MMC1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;U-Boot 2018.07-rc2-dirty (Aug 24 2018 - 10:03:53 +0530)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;CPU:&amp;nbsp;&amp;nbsp; Automotive temperature grade (-40C to 125C) at 48C&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Reset cause: WDOG&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Board: MX6-SabreSD&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DRAM:&amp;nbsp; 1 GiB&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;PMIC:&amp;nbsp; PFUZE100 ID=0x10&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Failed (-5)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;PCI:&amp;nbsp;&amp;nbsp; pcie phy link never came up&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;No panel detected: default to Hannstar-XGA&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Display: Hannstar-XGA (1024x768)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Net:&amp;nbsp;&amp;nbsp; FEC [PRIME]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Press SPACE to abort autoboot in 2 seconds&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;=&amp;gt; &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7 | VT102 | Offline | ttyUSB0&lt;/STRONG&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Karthik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 05:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820206#M126309</guid>
      <dc:creator>karthikas</dc:creator>
      <dc:date>2018-08-27T05:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot standalone application in sabre SD board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820207#M126310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Environment of my Example:&lt;/P&gt;&lt;P&gt;MCIMX6D6AVT08AD + AI EVB&lt;/P&gt;&lt;P&gt;The address of my example is the start of the OCRAM, as pic shows.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="ROM&amp;amp;RAM.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68961i805EE01E6B992CD8/image-size/large?v=v2&amp;amp;px=999" role="button" title="ROM&amp;amp;RAM.png" alt="ROM&amp;amp;RAM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your log, you may load the .bin to a wrong place, you can check the&amp;nbsp; chip RM to find a right one.&lt;/P&gt;&lt;P&gt;Not sure about this, hope it will work, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 06:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820207#M126310</guid>
      <dc:creator>nxf45220</dc:creator>
      <dc:date>2018-08-27T06:06:19Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot standalone application in sabre SD board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820208#M126311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually as per our board environment (printenv) the loadADDR is 0x12000000, thats why I chosen this address, On what basis this address can be selected, and if i choose an address which are places i need to update address in u-boot source code.&lt;/P&gt;&lt;P&gt;Can you give some brief steps to create our own standalone program, and run it on u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 08:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-standalone-application-in-sabre-SD-board/m-p/820208#M126311</guid>
      <dc:creator>karthikas</dc:creator>
      <dc:date>2018-08-27T08:59:46Z</dc:date>
    </item>
  </channel>
</rss>