<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRepetitive Kernel logo in sabresd kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Repetitive-Kernel-logo-in-sabresd-kernel/m-p/819374#M126205</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I am using sabresd reference board, and android O source from nxp.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While booting up I am seeing linux tux penguin logo at top right corner.&lt;/P&gt;&lt;P&gt;I am seeing 4 penguins, but I want to show only one,&lt;/P&gt;&lt;P&gt;1. How can I do that.&lt;/P&gt;&lt;P&gt;2. How can i change the position of it, like if I want to put it into middle of the screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mrigendra Chaubey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Aug 2018 13:35:42 GMT</pubDate>
    <dc:creator>mrigendra_chaub</dc:creator>
    <dc:date>2018-08-23T13:35:42Z</dc:date>
    <item>
      <title>Repetitive Kernel logo in sabresd kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Repetitive-Kernel-logo-in-sabresd-kernel/m-p/819374#M126205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I am using sabresd reference board, and android O source from nxp.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While booting up I am seeing linux tux penguin logo at top right corner.&lt;/P&gt;&lt;P&gt;I am seeing 4 penguins, but I want to show only one,&lt;/P&gt;&lt;P&gt;1. How can I do that.&lt;/P&gt;&lt;P&gt;2. How can i change the position of it, like if I want to put it into middle of the screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mrigendra Chaubey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 13:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Repetitive-Kernel-logo-in-sabresd-kernel/m-p/819374#M126205</guid>
      <dc:creator>mrigendra_chaub</dc:creator>
      <dc:date>2018-08-23T13:35:42Z</dc:date>
    </item>
    <item>
      <title>Re: Repetitive Kernel logo in sabresd kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Repetitive-Kernel-logo-in-sabresd-kernel/m-p/819375#M126206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mrigendra Chaubey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The penguin (named Tux, and the Linux mascot) is shown on the Kernel splash screen and one is shown for each core, so you are most likely running the i.MX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are a couple of threads where the topic of changing the Kernel Splash screen is discussed, as for example:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/960347?commentID=960347#comment-960347"&gt;https://community.nxp.com/message/960347?commentID=960347#comment-960347&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is not a simple guide on how to do this but perhaps this or other threads on the community may be of help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 20:14:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Repetitive-Kernel-logo-in-sabresd-kernel/m-p/819375#M126206</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-08-28T20:14:29Z</dc:date>
    </item>
  </channel>
</rss>