<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: using fsl-sdcard-partition.sh in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/using-fsl-sdcard-partition-sh/m-p/818983#M126172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which Android version and i.MX device are&amp;nbsp;you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you completely&amp;nbsp;sure that you installed&amp;nbsp;gdisk?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you installed al the packages specified in the AOSP webpage?&amp;nbsp;&lt;A class="link-titled" href="https://source.android.com/setup/build/initializing" title="https://source.android.com/setup/build/initializing"&gt;Establishing a Build Environment &amp;nbsp;|&amp;nbsp; Android Open Source Project&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please share with us the command that you used to run the fsl-sdcard-partition.sh script?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jun 2018 20:19:16 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-06-26T20:19:16Z</dc:date>
    <item>
      <title>using fsl-sdcard-partition.sh</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-fsl-sdcard-partition-sh/m-p/818982#M126171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to flash the SD card with the provided bash script, however the 'gdd' command is not found. I have installed all of the packages specified in the Android Users Guide under section 2.1 - Setting up your computer using apt-get, however gdd is not a command&amp;nbsp;my computer is recognizing. Does anyone know which package I need to install?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 15:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-fsl-sdcard-partition-sh/m-p/818982#M126171</guid>
      <dc:creator>lmilla13</dc:creator>
      <dc:date>2018-06-26T15:55:43Z</dc:date>
    </item>
    <item>
      <title>Re: using fsl-sdcard-partition.sh</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-fsl-sdcard-partition-sh/m-p/818983#M126172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which Android version and i.MX device are&amp;nbsp;you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you completely&amp;nbsp;sure that you installed&amp;nbsp;gdisk?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you installed al the packages specified in the AOSP webpage?&amp;nbsp;&lt;A class="link-titled" href="https://source.android.com/setup/build/initializing" title="https://source.android.com/setup/build/initializing"&gt;Establishing a Build Environment &amp;nbsp;|&amp;nbsp; Android Open Source Project&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please share with us the command that you used to run the fsl-sdcard-partition.sh script?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 20:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-fsl-sdcard-partition-sh/m-p/818983#M126172</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-06-26T20:19:16Z</dc:date>
    </item>
    <item>
      <title>Re: using fsl-sdcard-partition.sh</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-fsl-sdcard-partition-sh/m-p/818984#M126173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It turns out gdd is an OSX homebrew because the dd on osx doesn't work quite the same as GNU's dd.&amp;nbsp;Or something like that. I switched all the gdd commands to dd in the script and it seems to be working now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 13:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-fsl-sdcard-partition-sh/m-p/818984#M126173</guid>
      <dc:creator>lmilla13</dc:creator>
      <dc:date>2018-06-27T13:44:32Z</dc:date>
    </item>
  </channel>
</rss>