<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: wayland image with QT5 fails to build on Yocto Rocko for i.mx8m</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/818351#M126082</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Richard Hu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you still having problems when baking the Qt5 image? I will try to reproduce the problem. It is odd that the xwayland is working correctly and the wayland distro is not, considering that xwayland has many more dependencies.&lt;/P&gt;&lt;P&gt;I’ll let you know if I find something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jul 2018 21:02:06 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-07-23T21:02:06Z</dc:date>
    <item>
      <title>wayland image with QT5 fails to build on Yocto Rocko for i.mx8m</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/818350#M126081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Sir:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I follow the step in "i.MX_Yocto_Project_User's_Guide" to build wayland image with QT5(not xwayland) for &amp;nbsp;i.MX8 MQuad EVK and it always fails on building QT example "quickcontrols/controls".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The instructions i give are as follows:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;DIV style="-en-clipboard: true;"&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b&amp;nbsp;imx-linux-rocko -m&amp;nbsp;imx-4.9.88-2.0.0_ga.xml&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt; &lt;SPAN&gt;repo sync -j8&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland&lt;/SPAN&gt; &lt;/P&gt;&lt;DIV style="-en-clipboard: true;"&gt;bitbake fsl-image-qt5-validation-imx&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error message is as follows:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: /home/pico/workspace2/yocto/yocto_tn_rocko/nxp/build-wayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/temp/run.do_compile.19906:1 exit 1 from 'exit 1'&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/pico/workspace2/yocto/yocto_tn_rocko/nxp/build-wayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/temp/log.do_compile.19906)&lt;BR /&gt;ERROR: Task (/home/pico/workspace2/yocto/yocto_tn_rocko/nxp/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 2654 tasks of which 0 didn't need to be rerun and 2 failed.&lt;BR /&gt;&lt;BR /&gt;Summary: 2 tasks failed:&lt;BR /&gt;&amp;nbsp; /home/pico/workspace2/yocto/yocto_tn_rocko/nxp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/opencv/opencv_3.4.bb:do_compile&lt;BR /&gt;&amp;nbsp; /home/pico/workspace2/yocto/yocto_tn_rocko/nxp/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile&lt;BR /&gt;Summary: There were 8 WARNING messages shown.&lt;BR /&gt;Summary: There were 3 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I upload the complete error log as an attachment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't encounter this problem when i build the xwayland image. It only happens on wayland.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 04:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/818350#M126081</guid>
      <dc:creator>richard_hu</dc:creator>
      <dc:date>2018-07-17T04:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: wayland image with QT5 fails to build on Yocto Rocko for i.mx8m</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/818351#M126082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Richard Hu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you still having problems when baking the Qt5 image? I will try to reproduce the problem. It is odd that the xwayland is working correctly and the wayland distro is not, considering that xwayland has many more dependencies.&lt;/P&gt;&lt;P&gt;I’ll let you know if I find something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 21:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/818351#M126082</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-07-23T21:02:06Z</dc:date>
    </item>
    <item>
      <title>Re: wayland image with QT5 fails to build on Yocto Rocko for i.mx8m</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/818352#M126083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Gusarambula:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After i "repo sync", and run the build again. This issue is gone.&lt;/P&gt;&lt;P&gt;Now, it can produce "fsl-image-qt5-validation" image with wayland backend.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank for your help~!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 05:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/818352#M126083</guid>
      <dc:creator>richard_hu</dc:creator>
      <dc:date>2018-07-25T05:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: wayland image with QT5 fails to build on Yocto Rocko for i.mx8m</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/1184528#M165026</link>
      <description>&lt;P&gt;Hello, I have the same issue.&lt;BR /&gt;&lt;BR /&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-zeus -m imx-5.4.47-2.2.0.xml&lt;BR /&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b imxImageFull&lt;BR /&gt;bitbake imx-image-full&lt;/P&gt;&lt;P&gt;gives this error and exit.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;...sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile&amp;nbsp; failed with exit code '1'&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But I can build&amp;nbsp;imx-image-multimedia successfully. I also tried bitbake -c clean but nothing changed. What sould I do?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Nov 2020 14:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wayland-image-with-QT5-fails-to-build-on-Yocto-Rocko-for-i-mx8m/m-p/1184528#M165026</guid>
      <dc:creator>brsmnc</dc:creator>
      <dc:date>2020-11-17T14:02:32Z</dc:date>
    </item>
  </channel>
</rss>