<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RAM type supported by i.MX 6ULL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817872#M126018</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes these memory types also may be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jul 2018 01:19:26 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-07-19T01:19:26Z</dc:date>
    <item>
      <title>RAM type supported by i.MX 6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817869#M126015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;For the redesign of a cost-sensitive industrial application, (no display, only some serial, Can, Eth) we are evaluating i.MX6ULL processor;&amp;nbsp; the choice is based by attempt to minimize the effort/cost for porting the code of the actual version, developed on a linux embedded platform.&lt;/P&gt;&lt;P&gt;The RAM (DDR2 or DDR3) is the largest cost item in the BOM... so to minimize the cost we would like to mount the minimal quantity and the cheapest type of RAM. The datasheet isn't clear about all the RAM types supported.&lt;/P&gt;&lt;P&gt;I know that recent RAM types are cheapest, and the minimal density are growing... but if anyone has suggestion, we &lt;SPAN class=""&gt;&lt;SPAN class="" title=""&gt;would be very grateful&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class="" title=""&gt;Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Massimo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 07:44:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817869#M126015</guid>
      <dc:creator>mp-effegi</dc:creator>
      <dc:date>2018-07-17T07:44:47Z</dc:date>
    </item>
    <item>
      <title>Re: RAM type supported by i.MX 6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817870#M126016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, i.MX6UL MMDC supports only DDR3(L) or LPDDR2.&lt;/P&gt;&lt;P&gt;For cost sensitive applications one can consider running applications from&lt;/P&gt;&lt;P&gt;NOR flashes connected to EMI, QSPI or OCRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 11:26:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817870#M126016</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-18T11:26:52Z</dc:date>
    </item>
    <item>
      <title>Re: RAM type supported by i.MX 6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817871#M126017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, Igor&lt;/P&gt;&lt;P&gt;But if I want to maintain RAM , can I use slower DDR3L, for example 666MHz or 800MHz instead of Micron 933MHz type used in the evaluation board MCIMX6ULL-CM? The datasheet says that clock frequency for DDRx is 400MHz...&lt;SPAN style="font-family: ArialMT; font-size: 9pt; color: #000000; font-style: normal; font-variant: normal;"&gt;&lt;BR style="font-style: normal; font-variant: normal; font-weight: normal; letter-spacing: normal; line-height: normal; orphans: 2; text-align: -webkit-auto; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-size-adjust: auto; -webkit-text-stroke-width: 0px;" /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Massimo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 13:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817871#M126017</guid>
      <dc:creator>mp-effegi</dc:creator>
      <dc:date>2018-07-18T13:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: RAM type supported by i.MX 6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817872#M126018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes these memory types also may be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 01:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-type-supported-by-i-MX-6ULL/m-p/817872#M126018</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-19T01:19:26Z</dc:date>
    </item>
  </channel>
</rss>