<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: forcing a first time boot on Android for the iMX51 EVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145996#M126</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;My andorid-r8 worked normally. I guess there is something wrong in your compilation. If you want to use android-r8, you must use linux kernel-2.6.31 and compile it with Freescal compiler. I used kernel-2.6.28 for android-r8 and got the same error like you met. &lt;/SPAN&gt;&lt;CITE&gt;Rafael G. Lopez said:&lt;/CITE&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/forcing-a-first-time-boot-on?commentId=4103961%3AComment%3A2197&amp;amp;xg_source=msg_com_forum#4103961Comment2197"&gt;&lt;DIV&gt;Jack:&lt;BR /&gt; &lt;BR /&gt;Thank you. It works.&lt;BR /&gt;I also received this tip from the technical contact at Freescale.&lt;BR /&gt;However, after removing the calibration file, it did go through touch screen calibration, but then something else got wrecked, since Android would get stuck during loading, and it did not get to the main screen.&lt;BR /&gt;&lt;BR /&gt;I had to erase the SD card and do a clean installation, which did go through touchscreen calibration.&lt;BR /&gt;&lt;BR /&gt;I guess these are the growing pains of working with the iMX51 for the first time, along with Android, and the touchscreen feature. Too many new things at the same time.&lt;BR /&gt;&lt;BR /&gt;Rafael Lopez&lt;BR /&gt;&lt;BR /&gt;&lt;CITE&gt;jack kang said:&lt;/CITE&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/forcing-a-first-time-boot-on?commentId=4103961%3AComment%3A2194&amp;amp;xg_source=msg_com_forum#4103961Comment2194"&gt;&lt;DIV&gt;First you must move out the file: /data/system/calibration, then add calibration in your start env, the calibration cross will be appeared on your touch screen.&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 01 Aug 2010 15:06:02 GMT</pubDate>
    <dc:creator>Jackrun2000</dc:creator>
    <dc:date>2010-08-01T15:06:02Z</dc:date>
    <item>
      <title>forcing a first time boot on Android for the iMX51 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145993#M123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Can anyone help me figure out how to force an iMX51 EVK to do a first time boot on Android R8?&lt;/SPAN&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;I need to do touch screen calibration again.&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;Thank you.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jul 2010 23:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145993#M123</guid>
      <dc:creator>RafaelG_Lopez</dc:creator>
      <dc:date>2010-07-21T23:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: forcing a first time boot on Android for the iMX51 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145994#M124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;First you must move out the file: /data/system/calibration, then add calibration in your start env, the calibration cross will be appeared on your touch screen.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Jul 2010 02:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145994#M124</guid>
      <dc:creator>Jackrun2000</dc:creator>
      <dc:date>2010-07-31T02:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: forcing a first time boot on Android for the iMX51 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145995#M125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Jack:  Thank you. It works. I also received this tip from the technical contact at Freescale. However, after removing the calibration file, it did go through touch screen calibration, but then something else got wrecked, since Android would get stuck during loading, and it did not get to the main screen.  I had to erase the SD card and do a clean installation, which did go through touchscreen calibration.  I guess these are the growing pains of working with the iMX51 for the first time, along with Android, and the touchscreen feature. Too many new things at the same time.  Rafael Lopez &lt;/SPAN&gt;&lt;CITE&gt;jack kang said:&lt;/CITE&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/forcing-a-first-time-boot-on?commentId=4103961%3AComment%3A2194&amp;amp;xg_source=msg_com_forum#4103961Comment2194"&gt;&lt;DIV&gt;First you must move out the file: /data/system/calibration, then add calibration in your start env, the calibration cross will be appeared on your touch screen.&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Aug 2010 04:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145995#M125</guid>
      <dc:creator>RafaelG_Lopez</dc:creator>
      <dc:date>2010-08-01T04:24:00Z</dc:date>
    </item>
    <item>
      <title>Re: forcing a first time boot on Android for the iMX51 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145996#M126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;My andorid-r8 worked normally. I guess there is something wrong in your compilation. If you want to use android-r8, you must use linux kernel-2.6.31 and compile it with Freescal compiler. I used kernel-2.6.28 for android-r8 and got the same error like you met. &lt;/SPAN&gt;&lt;CITE&gt;Rafael G. Lopez said:&lt;/CITE&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/forcing-a-first-time-boot-on?commentId=4103961%3AComment%3A2197&amp;amp;xg_source=msg_com_forum#4103961Comment2197"&gt;&lt;DIV&gt;Jack:&lt;BR /&gt; &lt;BR /&gt;Thank you. It works.&lt;BR /&gt;I also received this tip from the technical contact at Freescale.&lt;BR /&gt;However, after removing the calibration file, it did go through touch screen calibration, but then something else got wrecked, since Android would get stuck during loading, and it did not get to the main screen.&lt;BR /&gt;&lt;BR /&gt;I had to erase the SD card and do a clean installation, which did go through touchscreen calibration.&lt;BR /&gt;&lt;BR /&gt;I guess these are the growing pains of working with the iMX51 for the first time, along with Android, and the touchscreen feature. Too many new things at the same time.&lt;BR /&gt;&lt;BR /&gt;Rafael Lopez&lt;BR /&gt;&lt;BR /&gt;&lt;CITE&gt;jack kang said:&lt;/CITE&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/forcing-a-first-time-boot-on?commentId=4103961%3AComment%3A2194&amp;amp;xg_source=msg_com_forum#4103961Comment2194"&gt;&lt;DIV&gt;First you must move out the file: /data/system/calibration, then add calibration in your start env, the calibration cross will be appeared on your touch screen.&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Aug 2010 15:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/forcing-a-first-time-boot-on-Android-for-the-iMX51-EVK/m-p/145996#M126</guid>
      <dc:creator>Jackrun2000</dc:creator>
      <dc:date>2010-08-01T15:06:02Z</dc:date>
    </item>
  </channel>
</rss>