<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Adding spi slave support for imx8qm evaluation board with Yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-spi-slave-support-for-imx8qm-evaluation-board-with-Yocto/m-p/817406#M125942</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I need to write an spi slave driver for an IMX8QuadMax evaluation board, using Yocto. I read that starting from kernel 4.13 Linux has also slave support in spi.c, but my board has an older version of the kernel. I wanted to know if I can update it to the needed version, and how. I am new to yocto and to driver development. Thank you in advance for your support!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Oct 2018 09:43:50 GMT</pubDate>
    <dc:creator>s233199</dc:creator>
    <dc:date>2018-10-02T09:43:50Z</dc:date>
    <item>
      <title>Adding spi slave support for imx8qm evaluation board with Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-spi-slave-support-for-imx8qm-evaluation-board-with-Yocto/m-p/817406#M125942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I need to write an spi slave driver for an IMX8QuadMax evaluation board, using Yocto. I read that starting from kernel 4.13 Linux has also slave support in spi.c, but my board has an older version of the kernel. I wanted to know if I can update it to the needed version, and how. I am new to yocto and to driver development. Thank you in advance for your support!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 09:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-spi-slave-support-for-imx8qm-evaluation-board-with-Yocto/m-p/817406#M125942</guid>
      <dc:creator>s233199</dc:creator>
      <dc:date>2018-10-02T09:43:50Z</dc:date>
    </item>
    <item>
      <title>Re: Adding spi slave support for imx8qm evaluation board with Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-spi-slave-support-for-imx8qm-evaluation-board-with-Yocto/m-p/817407#M125943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erica&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX8QuadMax processor is not officially launched and there is no full support for it yet.&lt;/P&gt;&lt;P&gt;One can try to add slave support using its driver sources on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-fsl-lpspi.c?h=imx_4.9.51_imx8_beta2" title="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-fsl-lpspi.c?h=imx_4.9.51_imx8_beta2"&gt;spi-fsl-lpspi.c\spi\drivers - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and slave software for this module from other processors software packages, like&lt;/P&gt;&lt;P&gt;EVKB-IMXRT1050 SDK..devices/MIMXRT1052/drivers/fsl_lpspi.c&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or sect.4.LPSPI Slave Operation AN5320&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN5320.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5320.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Oct 2018 00:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-spi-slave-support-for-imx8qm-evaluation-board-with-Yocto/m-p/817407#M125943</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-04T00:24:53Z</dc:date>
    </item>
  </channel>
</rss>