<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FXOS8700 linux driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FXOS8700-linux-driver/m-p/817315#M125921</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;In our custom board we use FXOS8700. When I start&amp;nbsp;driver from fsl-arm-yocto-bsp (kernel 4.9.11), I see that&amp;nbsp;it creates only one input device and event from accelerometer and magnetometer are emitting from one source, so I can't use acc and mag devices simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modifyed fxos8700 driver to create two input devices - separately for acc and mag. I think it will be useful to share this patch :smileyhappy:.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jun 2018 07:36:48 GMT</pubDate>
    <dc:creator>maximkuk</dc:creator>
    <dc:date>2018-06-26T07:36:48Z</dc:date>
    <item>
      <title>FXOS8700 linux driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FXOS8700-linux-driver/m-p/817315#M125921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;In our custom board we use FXOS8700. When I start&amp;nbsp;driver from fsl-arm-yocto-bsp (kernel 4.9.11), I see that&amp;nbsp;it creates only one input device and event from accelerometer and magnetometer are emitting from one source, so I can't use acc and mag devices simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modifyed fxos8700 driver to create two input devices - separately for acc and mag. I think it will be useful to share this patch :smileyhappy:.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 07:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FXOS8700-linux-driver/m-p/817315#M125921</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-06-26T07:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 linux driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FXOS8700-linux-driver/m-p/817316#M125922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Or there is another version of this driver from here:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/330614"&gt;https://community.nxp.com/thread/330614&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 08:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FXOS8700-linux-driver/m-p/817316#M125922</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-06-26T08:50:55Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 linux driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FXOS8700-linux-driver/m-p/817317#M125923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The patch fixed my problem.Thank you&amp;nbsp;very much for sharing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2020 09:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FXOS8700-linux-driver/m-p/817317#M125923</guid>
      <dc:creator>pandaerliu</dc:creator>
      <dc:date>2020-01-14T09:58:52Z</dc:date>
    </item>
  </channel>
</rss>