<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8M's USB Port</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-s-USB-Port/m-p/816866#M125817</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi xu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using i.MX8 EVK and the mfgtool use USB3.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jun 2018 13:36:52 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-06-27T13:36:52Z</dc:date>
    <item>
      <title>IMX8M's USB Port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-s-USB-Port/m-p/816865#M125816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When download the Imx8m's Image, the Imx8m EVK board use the J901 USB TYPE-C conncector. I wonder when use the Mfgtool download the Image through this port , the usb is running USB2.0 or USB3.0? &amp;nbsp;When downloading Image, if only the usb1_dp and usb1_dn is needed, the other usb signals is not neceasary? Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 03:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-s-USB-Port/m-p/816865#M125816</guid>
      <dc:creator>xuyuanzhi</dc:creator>
      <dc:date>2018-06-26T03:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M's USB Port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-s-USB-Port/m-p/816866#M125817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi xu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using i.MX8 EVK and the mfgtool use USB3.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 13:36:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-s-USB-Port/m-p/816866#M125817</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-06-27T13:36:52Z</dc:date>
    </item>
  </channel>
</rss>