<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 OCOTP_SW_STICKY modification</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/OCOTP-SW-STICKY-modification/m-p/816845#M125812</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to set the FIELD_RETURN_LOCK bit at OCOTP_SW_STICKY register.&lt;/P&gt;&lt;P&gt;When I set the FIELD_RETURN_LOCK in U-BOOT phase, it is able to set to 1.&lt;/P&gt;&lt;P&gt;But, when I set the FIELD_RETURN_LOCK in Linux phase, it is not able to set to 1.&lt;/P&gt;&lt;P&gt;Why I am not able to write the OCOTP_SW_STICKY register at linux phase?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;My environment&amp;gt;&lt;/P&gt;&lt;P&gt;BSP version = L4.1.15_2.0.0_ga&lt;/P&gt;&lt;P&gt;Board = SABRE-AI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;My test result&amp;gt;&lt;/P&gt;&lt;P&gt;(1) case of U-BOOT&lt;/P&gt;&lt;P&gt;=&amp;gt; md.l 0x21bc050 1&lt;BR /&gt;021bc050: 00000018&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ....&lt;BR /&gt;=&amp;gt; mw.l 0x21bc050 0x00000004&lt;BR /&gt;=&amp;gt; md.l 0x21bc050 1&lt;BR /&gt;021bc050: 0000001c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) case of Linux&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# /unit_tests/memtool -32 0x21bc050 1&lt;BR /&gt;Reading 0x1 count starting at address 0x021BC050&lt;/P&gt;&lt;P&gt;0x021BC050:&amp;nbsp; 00000018&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# /unit_tests/memtool -32 0x21bc050=0x00000004&lt;BR /&gt;Writing 32-bit value 0x4 to address 0x021BC050&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# /unit_tests/memtool -32 0x21bc050 1&lt;BR /&gt;Reading 0x1 count starting at address 0x021BC050&lt;/P&gt;&lt;P&gt;0x021BC050:&amp;nbsp; 00000018&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Oct 2018 05:38:57 GMT</pubDate>
    <dc:creator>Kazuma_Sasaki</dc:creator>
    <dc:date>2018-10-02T05:38:57Z</dc:date>
    <item>
      <title>OCOTP_SW_STICKY modification</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OCOTP-SW-STICKY-modification/m-p/816845#M125812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to set the FIELD_RETURN_LOCK bit at OCOTP_SW_STICKY register.&lt;/P&gt;&lt;P&gt;When I set the FIELD_RETURN_LOCK in U-BOOT phase, it is able to set to 1.&lt;/P&gt;&lt;P&gt;But, when I set the FIELD_RETURN_LOCK in Linux phase, it is not able to set to 1.&lt;/P&gt;&lt;P&gt;Why I am not able to write the OCOTP_SW_STICKY register at linux phase?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;My environment&amp;gt;&lt;/P&gt;&lt;P&gt;BSP version = L4.1.15_2.0.0_ga&lt;/P&gt;&lt;P&gt;Board = SABRE-AI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;My test result&amp;gt;&lt;/P&gt;&lt;P&gt;(1) case of U-BOOT&lt;/P&gt;&lt;P&gt;=&amp;gt; md.l 0x21bc050 1&lt;BR /&gt;021bc050: 00000018&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ....&lt;BR /&gt;=&amp;gt; mw.l 0x21bc050 0x00000004&lt;BR /&gt;=&amp;gt; md.l 0x21bc050 1&lt;BR /&gt;021bc050: 0000001c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) case of Linux&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# /unit_tests/memtool -32 0x21bc050 1&lt;BR /&gt;Reading 0x1 count starting at address 0x021BC050&lt;/P&gt;&lt;P&gt;0x021BC050:&amp;nbsp; 00000018&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# /unit_tests/memtool -32 0x21bc050=0x00000004&lt;BR /&gt;Writing 32-bit value 0x4 to address 0x021BC050&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# /unit_tests/memtool -32 0x21bc050 1&lt;BR /&gt;Reading 0x1 count starting at address 0x021BC050&lt;/P&gt;&lt;P&gt;0x021BC050:&amp;nbsp; 00000018&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 05:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OCOTP-SW-STICKY-modification/m-p/816845#M125812</guid>
      <dc:creator>Kazuma_Sasaki</dc:creator>
      <dc:date>2018-10-02T05:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: OCOTP_SW_STICKY modification</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OCOTP-SW-STICKY-modification/m-p/816846#M125813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi technical support team,&lt;/P&gt;&lt;P&gt;Do you have any update?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 15:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OCOTP-SW-STICKY-modification/m-p/816846#M125813</guid>
      <dc:creator>Kazuma_Sasaki</dc:creator>
      <dc:date>2018-10-09T15:09:38Z</dc:date>
    </item>
  </channel>
</rss>