<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Motion Control using iMX7 SoM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Motion-Control-using-iMX7-SoM/m-p/816373#M125752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;It looks like that your servo motor is step-motor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;This motor requires generates various frequency for signal PUL. Maximum frequency for step motors is 1000Hz - 5000Hz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Usually &lt;SPAN style="color: black;"&gt;Flextimer module or system timer is used for this task.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Aug 2018 09:14:59 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2018-08-07T09:14:59Z</dc:date>
    <item>
      <title>Motion Control using iMX7 SoM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Motion-Control-using-iMX7-SoM/m-p/816372#M125751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the iMX7 Dual SoM from Toradex in a design. I wish to generate PUL/DIR control signals for controlling a servo motor from this. The reference manual mentions the FlexTimer Module as well as a PWM module separately.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While the Flextimer module mentions that it can be used to generate PWM signals for motor control, the PWM sections mentions that it has been optimized to generate Audio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So what should I refer to if I need to generate motion profiles to control a servo motor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2018 07:48:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Motion-Control-using-iMX7-SoM/m-p/816372#M125751</guid>
      <dc:creator>DeepakKukreja</dc:creator>
      <dc:date>2018-08-06T07:48:59Z</dc:date>
    </item>
    <item>
      <title>Re: Motion Control using iMX7 SoM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Motion-Control-using-iMX7-SoM/m-p/816373#M125752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;It looks like that your servo motor is step-motor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;This motor requires generates various frequency for signal PUL. Maximum frequency for step motors is 1000Hz - 5000Hz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Usually &lt;SPAN style="color: black;"&gt;Flextimer module or system timer is used for this task.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 09:14:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Motion-Control-using-iMX7-SoM/m-p/816373#M125752</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-08-07T09:14:59Z</dc:date>
    </item>
  </channel>
</rss>