<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6 UART time between bytes</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-UART-time-between-bytes/m-p/815323#M125609</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, it is defined by SOC hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Dec 2018 23:14:58 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-12-19T23:14:58Z</dc:date>
    <item>
      <title>iMX6 UART time between bytes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-UART-time-between-bytes/m-p/815322#M125608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible configure the time between bytes in a iMX6 UART?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could no find a register in iMX6 UART to define the time between bytes when the UART TxFifo is filled out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it defined by SOC hardware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 05:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-UART-time-between-bytes/m-p/815322#M125608</guid>
      <dc:creator>joseluiszabalz1</dc:creator>
      <dc:date>2018-12-19T05:54:12Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 UART time between bytes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-UART-time-between-bytes/m-p/815323#M125609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, it is defined by SOC hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 23:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-UART-time-between-bytes/m-p/815323#M125609</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-19T23:14:58Z</dc:date>
    </item>
  </channel>
</rss>