<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8qxp in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp/m-p/814826#M125539</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check, If you are booting for SD1 the SW2&amp;nbsp; D1,D2 must be ON D3,D4 OFF.&amp;nbsp; if you are on eMMC D3 must be ON all rest OFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Aug 2018 15:01:29 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-08-23T15:01:29Z</dc:date>
    <item>
      <title>imx8qxp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp/m-p/814825#M125538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have i.MX 8QuadXPlus MEK CPU Board. i am trying to flash board using fsl-image-validation-imx-xwayland-imx8qxpmek.sdcard image by following command.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;sudo dd if=fsl-image-validation-imx-xwayland-imx8qxpmek.sdcard of=/dev/sdb bs=1M conv=fsync&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;it create partition and copy rootfs, Image and .dtb successfully.&lt;/P&gt;&lt;P&gt;configure sw2 1100.&lt;/P&gt;&lt;P&gt;but when i am using this sd card for boot up there is no console and uboot shell come.&lt;/P&gt;&lt;P&gt;when i am flash flash.bin image by following command&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;sudo dd if=iMX8QM/flash.bin of=/dev/sdb bs=1k seek=33&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;it blink d28 d40 led continuously but still log and u-boot shell not seen.&lt;/P&gt;&lt;P&gt;so please help me to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 12:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp/m-p/814825#M125538</guid>
      <dc:creator>arjun_salariya</dc:creator>
      <dc:date>2018-08-22T12:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp/m-p/814826#M125539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check, If you are booting for SD1 the SW2&amp;nbsp; D1,D2 must be ON D3,D4 OFF.&amp;nbsp; if you are on eMMC D3 must be ON all rest OFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 15:01:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp/m-p/814826#M125539</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-08-23T15:01:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp/m-p/814827#M125540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arjun,&lt;/P&gt;&lt;P&gt;I had a similar problem with same board. There were two causes:&lt;/P&gt;&lt;P&gt;- I was using the wrong /dev/sd* device for "dd" command, since my card reader mounted several /dev/sd* devices in linux file system,&lt;/P&gt;&lt;P&gt;- the SDcart was not very well inserted in MEK SDcard slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works perfectly now&lt;/P&gt;&lt;P&gt;hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 11:53:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp/m-p/814827#M125540</guid>
      <dc:creator>LaurentBardet</dc:creator>
      <dc:date>2019-06-13T11:53:50Z</dc:date>
    </item>
  </channel>
</rss>