<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Mainstream kernel support for imx6ul</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mainstream-kernel-support-for-imx6ul/m-p/814728#M125521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working in a project that will support Linux in imx6ul and atmel boards. So, I'd like to know what is the status of the imx6ul support in the mainstream kernels 4.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Fernando A. E.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Aug 2018 09:27:57 GMT</pubDate>
    <dc:creator>feae</dc:creator>
    <dc:date>2018-08-22T09:27:57Z</dc:date>
    <item>
      <title>Mainstream kernel support for imx6ul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainstream-kernel-support-for-imx6ul/m-p/814728#M125521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working in a project that will support Linux in imx6ul and atmel boards. So, I'd like to know what is the status of the imx6ul support in the mainstream kernels 4.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Fernando A. E.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 09:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainstream-kernel-support-for-imx6ul/m-p/814728#M125521</guid>
      <dc:creator>feae</dc:creator>
      <dc:date>2018-08-22T09:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: Mainstream kernel support for imx6ul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainstream-kernel-support-for-imx6ul/m-p/814729#M125522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fernando A. E.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are a couple of BSP Releases for NXP’s boards based on kernel 4.X. You can see them on the following link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX"&gt;https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also a Community BSP which is part of the Yocto Project and maintained by the community and this supports also 3&lt;SUP&gt;rd&lt;/SUP&gt; party boards and kernel revisions different than the BSP Releases which are somewhat limited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://freescale.github.io/"&gt;http://freescale.github.io/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend looking for these kernels when working on the i.MX6UL as porting a kernel from mainline may be time consuming.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 15:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainstream-kernel-support-for-imx6ul/m-p/814729#M125522</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-08-29T15:20:11Z</dc:date>
    </item>
  </channel>
</rss>