<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX53 sometimes hangs during boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814576#M125506</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think that the DDR is used at this stage of the boot process. And after 1 or more watchdog resets the board is finally booted then it runs perfectly. So the DDR seems to be OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;erratum ERR007080: Good point. Luckly our hw design takes care of this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Mogens&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jun 2018 10:42:29 GMT</pubDate>
    <dc:creator>mogenslauridsen</dc:creator>
    <dc:date>2018-06-27T10:42:29Z</dc:date>
    <item>
      <title>i.MX53 sometimes hangs during boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814573#M125503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the iMX53 (iMX538). Some of the boards we manufacture have problems booting. This might be something like 5% of the boards. After one or more reset caused by watchdog the board finally boots. This can delay the startup from 6 sec to 1-2 minutes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to find where it stops/hangs, and it happens while initializing the PLL's.&lt;/P&gt;&lt;P&gt;We use barebox but I have found the same sequence in u-boot:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First PLL3 is set to 400 MHz, then some peripheral is&amp;nbsp;switched to PLL3 and finally PLL3 is changed to 216 MHz.&lt;BR /&gt;Does anyone know why PLL3 first is set to 400MHz and later to 216MHz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See "imx5_setup_pll_400((void __iomem *)MX53_PLL2_BASE_ADDR);" and&lt;/P&gt;&lt;P&gt;"imx5_setup_pll_216((void __iomem *)MX53_PLL3_BASE_ADDR);" in the barebox code below.&lt;BR /&gt; &lt;BR /&gt; Our boards seem to boot fine if I change the code to set PLL3 to 216 MHz in the first place and don't change PLL3 later.&lt;BR /&gt; But does this have any side effects?&lt;BR /&gt; &lt;BR /&gt;Since this is only seen on some of the boards, I am guessing that something in some of the iMX53's doesn't run reliable at 400MHz, and hangs the boot process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;barebox: arch/arm/mach-imx/imx53.c:&lt;/P&gt;&lt;P&gt;void imx53_init_lowlevel_early(unsigned int cpufreq_mhz)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;void __iomem *ccm = (void __iomem *)MX53_CCM_BASE_ADDR;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;u32 r;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;imx5_init_lowlevel();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/*&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; * AIPS setup - Only setup MPROTx registers.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; * The PACR default values are good.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; * Set all MPROTx to be non-bufferable, trusted for R/W,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; * not forced to user-mode.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x77777777, MX53_AIPS1_BASE_ADDR + 0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x77777777, MX53_AIPS1_BASE_ADDR + 4);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x77777777, MX53_AIPS2_BASE_ADDR + 0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x77777777, MX53_AIPS2_BASE_ADDR + 4);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Gate of clocks to the peripherals first */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x3fffffff, ccm + MX5_CCM_CCGR0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00000000, ccm + MX5_CCM_CCGR1);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00000000, ccm + MX5_CCM_CCGR2);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00000000, ccm + MX5_CCM_CCGR3);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00030000, ccm + MX5_CCM_CCGR4);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00fff030, ccm + MX5_CCM_CCGR5);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x0f00030f, ccm + MX5_CCM_CCGR6);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00000000, ccm + MX53_CCM_CCGR7);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Switch ARM to step clock */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x4, ccm + MX5_CCM_CCSR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;if (cpufreq_mhz == 1000)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;imx5_setup_pll_1000((void __iomem *)MX53_PLL1_BASE_ADDR);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;imx5_setup_pll_800((void __iomem *)MX53_PLL1_BASE_ADDR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;imx5_setup_pll_400((void __iomem *)MX53_PLL3_BASE_ADDR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Switch peripheral to PLL3 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00015154, ccm + MX5_CCM_CBCMR);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x02888945 | (1&amp;lt;&amp;lt;16), ccm + MX5_CCM_CBCDR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* make sure change is effective */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while (readl(ccm + MX5_CCM_CDHIPR));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;imx5_setup_pll_400((void __iomem *)MX53_PLL2_BASE_ADDR);&amp;nbsp; &amp;lt;------------ 400MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Switch peripheral to PLL2 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r = 0x00808145 |&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;(2 &amp;lt;&amp;lt; 10) |&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;(0 &amp;lt;&amp;lt; 16) |&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;(1 &amp;lt;&amp;lt; 19);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(r, ccm + MX5_CCM_CBCDR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00016154, ccm + MX5_CCM_CBCMR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r = readl(ccm + MX5_CCM_CSCMR1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* change uart clk parent to pll2 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~MX5_CCM_CSCMR1_UART_CLK_SEL_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r |= 1 &amp;lt;&amp;lt; MX5_CCM_CSCMR1_UART_CLK_SEL_OFFSET;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* USB phy clock from osc */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~(1 &amp;lt;&amp;lt; MX5_CCM_CSCMR1_USB_PHY_CLK_SEL_OFFSET);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(r, ccm + MX5_CCM_CSCMR1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* make sure change is effective */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while (readl(ccm + MX5_CCM_CDHIPR));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;imx5_setup_pll_216((void __iomem *)MX53_PLL3_BASE_ADDR);&amp;nbsp; &amp;lt;------------ 216MHz&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;imx5_setup_pll_455((void __iomem *)MX53_PLL4_BASE_ADDR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Set the platform clock dividers */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0x00000124, MX53_ARM_BASE_ADDR + 0x14);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0, ccm + MX5_CCM_CACRR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Switch ARM back to PLL 1. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0, ccm + MX5_CCM_CCSR);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* make uart div = 6*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r = readl(ccm + MX5_CCM_CSCDR1);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~0x3f;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r |= 0x0a;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~MX5_CCM_CSCDR1_ESDHC1_MSHC1_CLK_PRED_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~MX5_CCM_CSCDR1_ESDHC1_MSHC1_CLK_PODF_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r |= 1 &amp;lt;&amp;lt; MX5_CCM_CSCDR1_ESDHC1_MSHC1_CLK_PRED_OFFSET;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~MX5_CCM_CSCDR1_ESDHC3_MX53_CLK_PRED_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~MX5_CCM_CSCDR1_ESDHC3_MX53_CLK_PODF_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r |= 1 &amp;lt;&amp;lt; MX5_CCM_CSCDR1_ESDHC3_MX53_CLK_PODF_OFFSET;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~MX5_CCM_CSCDR1_USBOH3_CLK_PRED_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r &amp;amp;= ~MX5_CCM_CSCDR1_USBOH3_CLK_PODF_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r |= 3 &amp;lt;&amp;lt; MX5_CCM_CSCDR1_USBOH3_CLK_PRED_OFFSET;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;r |= 1 &amp;lt;&amp;lt; MX5_CCM_CSCDR1_USBOH3_CLK_PODF_OFFSET;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(r, ccm + MX5_CCM_CSCDR1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Restore the default values in the Gate registers */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX5_CCM_CCGR0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX5_CCM_CCGR1);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX5_CCM_CCGR2);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX5_CCM_CCGR3);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX5_CCM_CCGR4);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX5_CCM_CCGR5);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX5_CCM_CCGR6);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0xffffffff, ccm + MX53_CCM_CCGR7);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;writel(0, ccm + MX5_CCM_CCDR);&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 12:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814573#M125503</guid>
      <dc:creator>mogenslauridsen</dc:creator>
      <dc:date>2018-06-25T12:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 sometimes hangs during boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814574#M125504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mogens&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to narrow down issue one can test ddr memory&lt;/P&gt;&lt;P&gt;Lab and Test Software (1)&lt;BR /&gt;DDR Stress tester kit for the i.MX51 and i.MX53&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/products/power-management/pmics/power-management-for-i.mx-application-processors/i.mx53-quick-start-board:IMX53QSB?tab=Design_Tools_Tab" title="https://www.nxp.com/products/power-management/pmics/power-management-for-i.mx-application-processors/i.mx53-quick-start-board:IMX53QSB?tab=Design_Tools_Tab"&gt;i.MX53 Quick Start Board|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and prolong POR up to 1 sec., to check if issue not caused by&lt;/P&gt;&lt;P&gt;clocks instability. Also may be useful to check ERR007080 erratum:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/errata/IMX53CE.pdf" title="https://www.nxp.com/docs/en/errata/IMX53CE.pdf"&gt;https://www.nxp.com/docs/en/errata/IMX53CE.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 23:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814574#M125504</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-25T23:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 sometimes hangs during boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814575#M125505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mogens,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think it is safer to setup the PLL3 only once to 216MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please prepare such patch and submit it to the Barebox list?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 23:53:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814575#M125505</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2018-06-26T23:53:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 sometimes hangs during boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814576#M125506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think that the DDR is used at this stage of the boot process. And after 1 or more watchdog resets the board is finally booted then it runs perfectly. So the DDR seems to be OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;erratum ERR007080: Good point. Luckly our hw design takes care of this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Mogens&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 10:42:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814576#M125506</guid>
      <dc:creator>mogenslauridsen</dc:creator>
      <dc:date>2018-06-27T10:42:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 sometimes hangs during boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814577#M125507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested the solution (use 216 MHz instead of 400MHz and only setting it once) on 10 boards. This seem to fix the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will submit a patch to the barebox list.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Mogens&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 10:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-sometimes-hangs-during-boot/m-p/814577#M125507</guid>
      <dc:creator>mogenslauridsen</dc:creator>
      <dc:date>2018-06-27T10:57:06Z</dc:date>
    </item>
  </channel>
</rss>