<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: U-boot variable substitution bug? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-variable-substitution-bug/m-p/814483#M125492</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure that there are no special characters among the command.&lt;BR /&gt;I mean if you copy the lines from text editor there may be some non-ascii characters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Oct 2018 07:39:33 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2018-10-19T07:39:33Z</dc:date>
    <item>
      <title>U-boot variable substitution bug?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-variable-substitution-bug/m-p/814482#M125491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using uboot-2016.03 for iMX6ul I'm having very odd behaving..&lt;/P&gt;&lt;P&gt;When I use&amp;nbsp;&lt;/P&gt;&lt;P&gt;bootcmd=nand read ${loadaddr} 0x500000 0xA00000;nand read ${fdt_addr} 0xF00000 0x100000;bootz ${loadaddr} - ${fdt_addr}&lt;/P&gt;&lt;P&gt;Auto boot hung after starting kernel message.&lt;/P&gt;&lt;P&gt;If I stop auto boot and type boot or similar, kernel starts OK.&lt;/P&gt;&lt;P&gt;BUT when I set&lt;/P&gt;&lt;P&gt;setenv bootcmd 'nand read ${loadaddr} 0x500000 0xA00000;nand read ${fdt_addr} 0xF00000 0x100000;bootz 0x80800000 - 0x83000000'&lt;/P&gt;&lt;P&gt;Kernel start OK by automatic boot or after power up.&lt;/P&gt;&lt;P&gt;So just replacing last substitution with real values everything works.&lt;/P&gt;&lt;P&gt;Can it be hush shell bug inside u-boot or some more space needed somewhere (CONFIG?)&lt;/P&gt;&lt;P&gt;Anyone seen similar?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 04:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-variable-substitution-bug/m-p/814482#M125491</guid>
      <dc:creator>juhapanula-ontt</dc:creator>
      <dc:date>2018-10-02T04:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot variable substitution bug?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-variable-substitution-bug/m-p/814483#M125492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure that there are no special characters among the command.&lt;BR /&gt;I mean if you copy the lines from text editor there may be some non-ascii characters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2018 07:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-variable-substitution-bug/m-p/814483#M125492</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-10-19T07:39:33Z</dc:date>
    </item>
  </channel>
</rss>