<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MMA8452 accelerometer sensor not working after device wakeup in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMA8452-accelerometer-sensor-not-working-after-device-wakeup/m-p/210600#M12549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; We are using MMA8452 accelerometer sensor in one of our android based target board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Driver for the acccelerometer (mma8452.c) working fine in normal conditions.Once the device entered into the sleep mode ,though the suspend and resume callback functions are getting called&amp;nbsp; we are not able to read the X,Y,Z register values through I2C.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This chip driver is registered as a input polled device.It doest have the interrupt handling capabilities.Is there any settings required to make driver to work porperly after wakeup in android.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Feb 2012 06:15:49 GMT</pubDate>
    <dc:creator>nit123</dc:creator>
    <dc:date>2012-02-14T06:15:49Z</dc:date>
    <item>
      <title>MMA8452 accelerometer sensor not working after device wakeup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMA8452-accelerometer-sensor-not-working-after-device-wakeup/m-p/210600#M12549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; We are using MMA8452 accelerometer sensor in one of our android based target board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Driver for the acccelerometer (mma8452.c) working fine in normal conditions.Once the device entered into the sleep mode ,though the suspend and resume callback functions are getting called&amp;nbsp; we are not able to read the X,Y,Z register values through I2C.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This chip driver is registered as a input polled device.It doest have the interrupt handling capabilities.Is there any settings required to make driver to work porperly after wakeup in android.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2012 06:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMA8452-accelerometer-sensor-not-working-after-device-wakeup/m-p/210600#M12549</guid>
      <dc:creator>nit123</dc:creator>
      <dc:date>2012-02-14T06:15:49Z</dc:date>
    </item>
  </channel>
</rss>