<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: how to build zImage for i.mx8mq</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/how-to-build-zImage-for-i-mx8mq/m-p/813440#M125389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kingplayer,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You would need to setup zImage as KERNEL_IMAGETYPE on the MACHINE configuration file for your board. The zImage is not defined for the i.MX8m which is why it’s prompting an error. I haven’t tried enabling it though, but it should be possible.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope this helps!&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Aug 2018 15:38:50 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-08-29T15:38:50Z</dc:date>
    <item>
      <title>how to build zImage for i.mx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-build-zImage-for-i-mx8mq/m-p/813439#M125388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi nxp,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I want&amp;nbsp; download zImage from ftp,and use nfs,but only Image build on imx8mq by defalut&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff; font-weight: bold;"&gt;Yocto Project&lt;/SPAN&gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed&amp;nbsp; imx-base.inc, &amp;nbsp;KERNEL_IMAGETYPE_mx8 = "Image"&lt;BR /&gt;&amp;nbsp;to&amp;nbsp;KERNEL_IMAGETYPE_mx8 = "zImage", then build error!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;build log:&lt;/P&gt;&lt;P&gt;| DEBUG: Executing shell function do_compile&lt;BR /&gt;| NOTE: make -j 4 HOSTCC=gcc -isystem/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/usr/lib -L/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E ARCH=arm64 zImage CC=aarch64-poky-linux-gcc -fuse-ld=bfd -ffile-prefix-map=/home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/git=/kernel-source/ LD=aarch64-poky-linux-ld.bfd LOADADDR=20008000&lt;BR /&gt;| GEN ./Makefile&lt;BR /&gt;| scripts/kconfig/conf --silentoldconfig Kconfig&lt;BR /&gt;| &lt;STRONG&gt;make[2]: *** No rule to make target `zImage'. Stop.&lt;/STRONG&gt;&lt;BR /&gt;| make[1]: *** [sub-make] Error 2&lt;BR /&gt;| make: *** [__sub-make] Error 2&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/droid/imx-yocto-bsp/build-xwayland/tmp/work/imx8mqevk-poky-linux/linux-imx/4.9.88-r0/temp/log.do_compile.7837)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how to build zImage for nfs use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 07:48:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-build-zImage-for-i-mx8mq/m-p/813439#M125388</guid>
      <dc:creator>kingplayer</dc:creator>
      <dc:date>2018-08-22T07:48:40Z</dc:date>
    </item>
    <item>
      <title>Re: how to build zImage for i.mx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-build-zImage-for-i-mx8mq/m-p/813440#M125389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kingplayer,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You would need to setup zImage as KERNEL_IMAGETYPE on the MACHINE configuration file for your board. The zImage is not defined for the i.MX8m which is why it’s prompting an error. I haven’t tried enabling it though, but it should be possible.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope this helps!&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 15:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-build-zImage-for-i-mx8mq/m-p/813440#M125389</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-08-29T15:38:50Z</dc:date>
    </item>
    <item>
      <title>Re: how to build zImage for i.mx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-build-zImage-for-i-mx8mq/m-p/813441#M125390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, it isn't possible to build a zImage for ARM64 platforms (such as the i.MX8MQ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is because it was decided in Linux not to add zImage support, so there's no way around it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An alternative is to compress the Image file (Image.gz) and then have the bootloader uncompress it before jumping into it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2018 08:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-build-zImage-for-i-mx8mq/m-p/813441#M125390</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2018-08-30T08:19:10Z</dc:date>
    </item>
  </channel>
</rss>