<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLinux support: fs encryption, CAN filtering, Watchdog?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812429#M125273</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the current Linux kernel fpr i.MX6 support:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Encrypting block devices and/or filesystems using hardware encryption via CAAM?&lt;/P&gt;&lt;P&gt;2) If not, encryption done by the kernel but using a key that is generated from the builtin hardware key or the master key from SNVS?&lt;/P&gt;&lt;P&gt;3) CAN-Filtering using the Flexcan interface?&lt;/P&gt;&lt;P&gt;4) Feeding the hardware watchdogs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Pointers to the relevant documentation for the Linux features are also very welcome.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Sep 2018 13:00:36 GMT</pubDate>
    <dc:creator>dominik_vogt_ex</dc:creator>
    <dc:date>2018-09-11T13:00:36Z</dc:date>
    <item>
      <title>Linux support: fs encryption, CAN filtering, Watchdog?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812429#M125273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the current Linux kernel fpr i.MX6 support:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Encrypting block devices and/or filesystems using hardware encryption via CAAM?&lt;/P&gt;&lt;P&gt;2) If not, encryption done by the kernel but using a key that is generated from the builtin hardware key or the master key from SNVS?&lt;/P&gt;&lt;P&gt;3) CAN-Filtering using the Flexcan interface?&lt;/P&gt;&lt;P&gt;4) Feeding the hardware watchdogs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Pointers to the relevant documentation for the Linux features are also very welcome.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2018 13:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812429#M125273</guid>
      <dc:creator>dominik_vogt_ex</dc:creator>
      <dc:date>2018-09-11T13:00:36Z</dc:date>
    </item>
    <item>
      <title>Re: Linux support: fs encryption, CAN filtering, Watchdog?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812430#M125274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi D. Vogt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for supported functionality one can look at nxp linux documentation&lt;/P&gt;&lt;P&gt;(Release Notes, Linux Manual) on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2018 23:02:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812430#M125274</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-11T23:02:37Z</dc:date>
    </item>
    <item>
      <title>Re: Linux support: fs encryption, CAN filtering, Watchdog?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812431#M125275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&amp;nbsp; Is the stuff in imx-yocto-L4.9.88_2.0.0.tar.gz what you mean?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reference manual in there says nothing about how the actual crypto algorithms are used.&amp;nbsp; As far as I understand, the kernel makes use of them automatically if you configure the device mapper to use them.&amp;nbsp; There must be some side channel to tell the crypto module which key to use.&amp;nbsp; Is there any further documentation on that topic?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2018 09:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812431#M125275</guid>
      <dc:creator>dominik_vogt_ex</dc:creator>
      <dc:date>2018-09-12T09:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: Linux support: fs encryption, CAN filtering, Watchdog?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812432#M125276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;also one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95700"&gt;Q&amp;amp;amp;A: Why is CAAM Driver Not Functioning in Linux for iMX6?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://events17.linuxfoundation.org/sites/events/files/slides/2017-02%20-%20ELC%20-%20Hudson%20-%20Linux%20Cryptographic%20Acceleration%20on%20an%20MX6.pdf" title="http://events17.linuxfoundation.org/sites/events/files/slides/2017-02%20-%20ELC%20-%20Hudson%20-%20Linux%20Cryptographic%20Acceleration%20on%20an%20MX6.pdf"&gt;http://events17.linuxfoundation.org/sites/events/files/slides/2017-02%20-%20ELC%20-%20Hudson%20-%20Linux%20Cryptographic…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.digi.com/resources/documentation/digidocs/90001546/reference/android/r_caam_android.htm" title="https://www.digi.com/resources/documentation/digidocs/90001546/reference/android/r_caam_android.htm"&gt;CAAM (Cryptographic Accelerator and Assurance Module)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2018 01:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-support-fs-encryption-CAN-filtering-Watchdog/m-p/812432#M125276</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-13T01:19:30Z</dc:date>
    </item>
  </channel>
</rss>