<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Device Descriptor failed in imx6ul in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812243#M125243</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using boot mode switches we are changing it to Download mode after that we are connecting USB otg 1 to PC(windows 10), then we are getting error (attached image check the highlighted in red). When we run mfgtool it is showing no device connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67489i7D320DA9B69C5449/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Aug 2018 08:06:52 GMT</pubDate>
    <dc:creator>chandraevolute</dc:creator>
    <dc:date>2018-08-24T08:06:52Z</dc:date>
    <item>
      <title>Device Descriptor failed in imx6ul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812241#M125241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We got our custom board for production, we are using USB OTG port to flash the kernel, rootfs and uboot using mfgtool.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When we change to download mode and connect the USB otg port to PC , it is throwing USB device discriptor failed in the device manager. Is there any solution for this problem. Using imx6ul processor and custom board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chandrasekhar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 06:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812241#M125241</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2018-08-22T06:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: Device Descriptor failed in imx6ul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812242#M125242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how did you change and what the error information? pls give me more detailed information about your issue, when you connect board to PC, pls check if the PC can detect the board or not, pls share your operation steps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 07:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812242#M125242</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-08-24T07:57:51Z</dc:date>
    </item>
    <item>
      <title>Re: Device Descriptor failed in imx6ul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812243#M125243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using boot mode switches we are changing it to Download mode after that we are connecting USB otg 1 to PC(windows 10), then we are getting error (attached image check the highlighted in red). When we run mfgtool it is showing no device connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67489i7D320DA9B69C5449/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 08:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812243#M125243</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2018-08-24T08:06:52Z</dc:date>
    </item>
    <item>
      <title>Re: Device Descriptor failed in imx6ul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812244#M125244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seemsn the PC couldn't detect the board, you can try to install the driver or change to another PC, if your PC detect board, you should find it from "Human Interface Devices", &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 08:47:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812244#M125244</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-08-24T08:47:16Z</dc:date>
    </item>
    <item>
      <title>Re: Device Descriptor failed in imx6ul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812245#M125245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We tried all the steps you have mentioned, still it is behaving the same way. We have 5 custom boards ,one board is working but rest of the boards are not working. Is there anything to be done on Hardware side??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 10:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Descriptor-failed-in-imx6ul/m-p/812245#M125245</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2018-08-24T10:07:20Z</dc:date>
    </item>
  </channel>
</rss>