<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i2s or SPDIF support in linux kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i2s-or-SPDIF-support-in-linux-kernel/m-p/210427#M12523</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, both are supported in kernel 2.6.31. which is available in our webpage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can confirm what drivers are available in our BSP by consulting the documentation, specifically the Linux Reference Manual.&lt;/P&gt;&lt;P&gt;SPDIF is explicitly shown in the BSP block diagram,&lt;/P&gt;&lt;P&gt;I2S's driver's file name is imx-ssi.c and it is meant to work with the SGTL5000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Oct 2012 21:41:49 GMT</pubDate>
    <dc:creator>4guin4g4</dc:creator>
    <dc:date>2012-10-09T21:41:49Z</dc:date>
    <item>
      <title>i2s or SPDIF support in linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2s-or-SPDIF-support-in-linux-kernel/m-p/210426#M12522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; background-color: #f0f4f7;"&gt;Is it available support for SPDIF or i2s in some linux kernel version for imx233 ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Oct 2012 13:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2s-or-SPDIF-support-in-linux-kernel/m-p/210426#M12522</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-10-05T13:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: i2s or SPDIF support in linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2s-or-SPDIF-support-in-linux-kernel/m-p/210427#M12523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, both are supported in kernel 2.6.31. which is available in our webpage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can confirm what drivers are available in our BSP by consulting the documentation, specifically the Linux Reference Manual.&lt;/P&gt;&lt;P&gt;SPDIF is explicitly shown in the BSP block diagram,&lt;/P&gt;&lt;P&gt;I2S's driver's file name is imx-ssi.c and it is meant to work with the SGTL5000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2012 21:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2s-or-SPDIF-support-in-linux-kernel/m-p/210427#M12523</guid>
      <dc:creator>4guin4g4</dc:creator>
      <dc:date>2012-10-09T21:41:49Z</dc:date>
    </item>
  </channel>
</rss>