<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx7 boot from eMMC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811974#M125217</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we're trying to boot a custom board with an imx7 and eMMC connected to USDHC3.&lt;/P&gt;&lt;P&gt;The board boots in manufacturing mode, and we're able to write the eMMC from linux loaded by the manufacturing tool.&lt;/P&gt;&lt;P&gt;We've checked the image written to mmcblk2boot0 is correct by reading it with the dd command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we reboot the board it's stays in manufacturing mode.&lt;/P&gt;&lt;P&gt;We see the boot ROM sending commands to the eMMC with the&amp;nbsp;347.22 KHz clock, but never switching to the 20MHz clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to read boot ROM errors from an imx7? For the imx6 it's been mentioned there's a boot ROM log buffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Cedric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Dec 2018 21:57:53 GMT</pubDate>
    <dc:creator>cedricjehasse</dc:creator>
    <dc:date>2018-12-18T21:57:53Z</dc:date>
    <item>
      <title>imx7 boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811974#M125217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we're trying to boot a custom board with an imx7 and eMMC connected to USDHC3.&lt;/P&gt;&lt;P&gt;The board boots in manufacturing mode, and we're able to write the eMMC from linux loaded by the manufacturing tool.&lt;/P&gt;&lt;P&gt;We've checked the image written to mmcblk2boot0 is correct by reading it with the dd command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we reboot the board it's stays in manufacturing mode.&lt;/P&gt;&lt;P&gt;We see the boot ROM sending commands to the eMMC with the&amp;nbsp;347.22 KHz clock, but never switching to the 20MHz clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to read boot ROM errors from an imx7? For the imx6 it's been mentioned there's a boot ROM log buffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Cedric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 21:57:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811974#M125217</guid>
      <dc:creator>cedricjehasse</dc:creator>
      <dc:date>2018-12-18T21:57:53Z</dc:date>
    </item>
    <item>
      <title>Re: imx7 boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811975#M125218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cedric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately reading ROM errors from an imx7 using boot ROM log buffer&lt;/P&gt;&lt;P&gt;is not documented ("not supported"), in general one can try to recheck boot settings&lt;/P&gt;&lt;P&gt;reading&amp;nbsp;SRC_SBMR1,2 registers with jtag and checking emmc data with logic&lt;/P&gt;&lt;P&gt;analyzer to find where error happens.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 01:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811975#M125218</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-19T01:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx7 boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811976#M125219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We got further into our debugging. It looks like the boot ROM is reading from eMMC.&lt;/P&gt;&lt;P&gt;The IVT in OCRAM looks ok, the IVT in DDR is corrupt and u-boot in DDR also looks ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've read this with jtag:&lt;/P&gt;&lt;P&gt;The IVT in OCRAM:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;(gdb) x /64xw 0x910400 &lt;BR /&gt;0x910400: 0x402000d1 0x87800000 0x00000000 0x877ff42c &lt;BR /&gt;0x910410: 0x877ff420 0x877ff400 0x00000000 0x00000000 &lt;BR /&gt;0x910420: 0x877ff000 0x00075000 0x00000000 0x40d401d2 &lt;BR /&gt;0x910430: 0x048c01cc 0x04003430 0x0500404f 0x88033630 &lt;BR /&gt;0x910440: 0x00000040 0x84033630 0x00000040 0x00103930 &lt;BR /&gt;0x910450: 0x02000000 0x00007a30 0x01100401 0xa0017a30 &lt;BR /&gt;0x910460: 0x03004080 0xa4017a30 0x20001000 0xa8017a30 &lt;BR /&gt;0x910470: 0x04001080 0x64007a30 0x46004000 0x90047a30 &lt;BR /&gt;0x910480: 0x01000000 0xd0007a30 0x01003500 0xd4007a30 &lt;BR /&gt;0x910490: 0x00000100 0xdc007a30 0x04003009 0xe0007a30 &lt;BR /&gt;0x9104a0: 0x00000804 0xe4007a30 0x06001100 0xf4007a30 &lt;BR /&gt;0x9104b0: 0x3f030000 0x00017a30 0x09110809 0x04017a30 &lt;BR /&gt;0x9104c0: 0x0d020700 0x08017a30 0x07040403 0x0c017a30 &lt;BR /&gt;0x9104d0: 0x06200000 0x10017a30 0x05020204 0x14017a30 &lt;BR /&gt;0x9104e0: 0x02020303 0x20017a30 0x03080000 0x80017a30 &lt;BR /&gt;0x9104f0: 0x20008000 0x84017a30 0x00010002 0x90017a30&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The IVT in DDR (every word has two bytes set to 0xff)&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;(gdb) x /64xw 0x877ff400 &lt;BR /&gt;0x877ff400: 0x40ff00ff 0x87ff00ff 0x00ff00ff 0x87fff4ff &lt;BR /&gt;0x877ff410: 0x87fff4ff 0x87fff4ff 0x00ff00ff 0x00ff00ff &lt;BR /&gt;0x877ff420: 0x87fff0ff 0x00ff50ff 0x00ff00ff 0x40ff01ff &lt;BR /&gt;0x877ff430: 0x04ff01ff 0x04ff34ff 0x05ff40ff 0x88ff36ff &lt;BR /&gt;0x877ff440: 0x00ff00ff 0x84ff36ff 0x00ff00ff 0x00ff39ff &lt;BR /&gt;0x877ff450: 0x02ff00ff 0x00ff7aff 0x01ff04ff 0xa0ff7aff &lt;BR /&gt;0x877ff460: 0x03ff40ff 0xa4ff7aff 0x20ff10ff 0xa8ff7aff &lt;BR /&gt;0x877ff470: 0x04ff10ff 0x64ff7aff 0x46ff40ff 0x90ff7aff &lt;BR /&gt;0x877ff480: 0x01ff00ff 0xd0ff7aff 0x01ff35ff 0xd4ff7aff &lt;BR /&gt;0x877ff490: 0x00ff01ff 0xdcff7aff 0x04ff30ff 0xe0ff7aff &lt;BR /&gt;0x877ff4a0: 0x00ff08ff 0xe4ff7aff 0x06ff11ff 0xf4ff7aff &lt;BR /&gt;0x877ff4b0: 0x3fff00ff 0x00ff7aff 0x09ff08ff 0x04ff7aff &lt;BR /&gt;0x877ff4c0: 0x0dff07ff 0x08ff7aff 0x07ff04ff 0x0cff7aff &lt;BR /&gt;0x877ff4d0: 0x06ff00ff 0x10ff7aff 0x05ff02ff 0x14ff7aff &lt;BR /&gt;0x877ff4e0: 0x02ff03ff 0x20ff7aff 0x03ff00ff 0x80ff7aff &lt;BR /&gt;0x877ff4f0: 0x20ff80ff 0x84ff7aff 0x00ff00ff 0x90ff7aff&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot in DDR:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;(gdb) x /64x 0x87800000 &lt;BR /&gt;0x87800000: 0xea0000b8 0xe59ff014 0xe59ff014 0xe59ff014 &lt;BR /&gt;0x87800010: 0xe59ff014 0xe59ff014 0xe59ff014 0xe59ff014 &lt;BR /&gt;0x87800020: 0x87800060 0x878000c0 0x87800120 0x87800180 &lt;BR /&gt;0x87800030: 0x878001e0 0x87800240 0x878002a0 0xdeadbeef &lt;BR /&gt;0x87800040: 0x0badc0de 0xe320f000 0xe320f000 0xe320f000 &lt;BR /&gt;0x87800050: 0xe320f000 0xe320f000 0xe320f000 0xe320f000 &lt;BR /&gt;0x87800060: 0xe51fd028 0xe58de000 0xe14fe000 0xe58de004 &lt;BR /&gt;0x87800070: 0xe3a0d013 0xe169f00d 0xe1a0e00f 0xe1b0f00e &lt;BR /&gt;0x87800080: 0xe24dd048 0xe88d1fff 0xe51f2050 0xe892000c &lt;BR /&gt;0x87800090: 0xe28d0048 0xe28d5034 0xe1a0100e 0xe885000f &lt;BR /&gt;0x878000a0: 0xe1a0000d 0xeb000c00 0xe320f000 0xe320f000 &lt;BR /&gt;0x878000b0: 0xe320f000 0xe320f000 0xe320f000 0xe320f000 &lt;BR /&gt;0x878000c0: 0xe51fd088 0xe58de000 0xe14fe000 0xe58de004 &lt;BR /&gt;0x878000d0: 0xe3a0d013 0xe169f00d 0xe1a0e00f 0xe1b0f00e &lt;BR /&gt;0x878000e0: 0xe24dd048 0xe88d1fff 0xe51f20b0 0xe892000c &lt;BR /&gt;0x878000f0: 0xe28d0048 0xe28d5034 0xe1a0100e 0xe885000f&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the IVT in DDR copied over from OCRAM? Or is it read a second time from eMMC?&lt;/P&gt;&lt;P&gt;Have you ever encountered an issue like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Cedric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 18:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811976#M125219</guid>
      <dc:creator>cedricjehasse</dc:creator>
      <dc:date>2018-12-19T18:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: imx7 boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811977#M125220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cedric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so had you run ddr test and updated image with new calibration coefficients&lt;/P&gt;&lt;P&gt;found from test:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V3.00&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does board boot fine to ddr using other methods, like sd or tftp.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Dec 2018 03:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7-boot-from-eMMC/m-p/811977#M125220</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-21T03:24:58Z</dc:date>
    </item>
  </channel>
</rss>