<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Audio jack output</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-jack-output/m-p/811300#M125117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is normal since Alsa is using the audio jack output as default audio card. You need to change this default configuration and select the Audio card that is assigned&amp;nbsp;to the HDMI audio. Using Linux, I made it as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$&amp;nbsp;gplay-1.0 test.mp4 --video-sink="kmssink" --audio-sink='alsasink device="hw:3,0"'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Nov 2018 21:22:24 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-11-30T21:22:24Z</dc:date>
    <item>
      <title>Audio jack output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-jack-output/m-p/811299#M125116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working on i.MX8M Evaluation kit and came across an issue, where there is audio output only from HDMI and no audio output from jack, when i flash Android binaries onto the Evaluation kit . As per the release note, it is stated that all the audio signals are routed to HDMI when a HDMI monitor is connected to the kit. Similarly when i flash Linux (4.9.88) binaries onto the same Evaluation kit, audio output is only from jack and not from HDMI. Can you please tell which factor is playing a major role on linux platform to get audio output from jack?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Deexith&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 05:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-jack-output/m-p/811299#M125116</guid>
      <dc:creator>deexithamba</dc:creator>
      <dc:date>2018-11-28T05:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: Audio jack output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-jack-output/m-p/811300#M125117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is normal since Alsa is using the audio jack output as default audio card. You need to change this default configuration and select the Audio card that is assigned&amp;nbsp;to the HDMI audio. Using Linux, I made it as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$&amp;nbsp;gplay-1.0 test.mp4 --video-sink="kmssink" --audio-sink='alsasink device="hw:3,0"'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2018 21:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-jack-output/m-p/811300#M125117</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-11-30T21:22:24Z</dc:date>
    </item>
  </channel>
</rss>