<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX7D - Cortex M4 - GPIO-SPEED</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Cortex-M4-GPIO-SPEED/m-p/811295#M125115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The GPIO module switching timings you observe are the realistic ones since these numbers include some software overhead, GPIO inter-module transfer timings etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try to increase the IPG_CLK_ROOT frequency on your own risk, however, it may cause the whole system to hang up.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Dec 2018 10:43:21 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2018-12-26T10:43:21Z</dc:date>
    <item>
      <title>IMX7D - Cortex M4 - GPIO-SPEED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Cortex-M4-GPIO-SPEED/m-p/811294#M125114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this time I'm trying to determine how fast the CortexM4 can / will handle GPIO reads/writes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A very simple IO-TOGGLE running on Bare-Metal (native) Cortex-M4.. shows me that it takes up-to +400ns to toggle an GPIO pin.&amp;nbsp; ( a high low / low high sequence ( square wave) takes +800ns ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see similar 'speeds' for reading ( iso writing) an GPIO pin !&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any possibility to improve ( speed this up) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;From the reference manual&amp;nbsp;I see that the peripheral clock is running at 24MHz, so I would expect this to be faster ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Worst case scenario ?&lt;SPAN&gt;&amp;nbsp;Can I increase the peripheral clock speed , without breaking either Linux or FreeRTOS.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Noel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 07:10:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Cortex-M4-GPIO-SPEED/m-p/811294#M125114</guid>
      <dc:creator>Noel_V</dc:creator>
      <dc:date>2018-12-19T07:10:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D - Cortex M4 - GPIO-SPEED</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Cortex-M4-GPIO-SPEED/m-p/811295#M125115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The GPIO module switching timings you observe are the realistic ones since these numbers include some software overhead, GPIO inter-module transfer timings etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try to increase the IPG_CLK_ROOT frequency on your own risk, however, it may cause the whole system to hang up.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2018 10:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-Cortex-M4-GPIO-SPEED/m-p/811295#M125115</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-12-26T10:43:21Z</dc:date>
    </item>
  </channel>
</rss>