<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIs eCSPI hardware identical between i.MX processors?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-eCSPI-hardware-identical-between-i-MX-processors/m-p/810869#M125069</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the eCSPI hardware within the i.MX8 identical to previous i.MX7/6 processors?&lt;BR /&gt;If the hardware is the same, are the software drivers also therefore identical for each processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason I ask is that I'd like to characterise the performance of the eCSPI interface on an i.MX8M, but presently only have an i.MX7D development board available. If I can make use of the eCSPI hardware/software on the i.MX7D and be confident that it's representative of the i.MX8M eCSPI then that'd save us some time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Nov 2018 20:28:12 GMT</pubDate>
    <dc:creator>michael_stanger</dc:creator>
    <dc:date>2018-11-28T20:28:12Z</dc:date>
    <item>
      <title>Is eCSPI hardware identical between i.MX processors?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-eCSPI-hardware-identical-between-i-MX-processors/m-p/810869#M125069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the eCSPI hardware within the i.MX8 identical to previous i.MX7/6 processors?&lt;BR /&gt;If the hardware is the same, are the software drivers also therefore identical for each processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason I ask is that I'd like to characterise the performance of the eCSPI interface on an i.MX8M, but presently only have an i.MX7D development board available. If I can make use of the eCSPI hardware/software on the i.MX7D and be confident that it's representative of the i.MX8M eCSPI then that'd save us some time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 20:28:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-eCSPI-hardware-identical-between-i-MX-processors/m-p/810869#M125069</guid>
      <dc:creator>michael_stanger</dc:creator>
      <dc:date>2018-11-28T20:28:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is eCSPI hardware identical between i.MX processors?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-eCSPI-hardware-identical-between-i-MX-processors/m-p/810870#M125070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right i.MX8M eCSPI module is the same as in i.MX6/7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 00:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-eCSPI-hardware-identical-between-i-MX-processors/m-p/810870#M125070</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-11-29T00:39:33Z</dc:date>
    </item>
  </channel>
</rss>